Device Status

Use the Predix Edge Technician Console Device Status page to view information about the device, monitor the device, and edit settings.

When you sign into Predix Edge Technician Console, the Device Status page is displayed. This page displays information about the device and also allows you to perform certain actions.

Table 1. Device Information
Details
  • Last Restart – Date and time the device was last restarted.
  • Model – Device model.
  • Processor – Processor installed on the device.
  • Number of Cores – Number of cores installed on the device.
  • Polling Interval – The time interval set to synchronize how often the edge devices communicate with Edge Manager in the cloud.
  • Operating System – The operating system running on the device.
  • Last Updated – Displays the date the host operating system was last updated.
Device
  • ID – The device ID.
  • Container Enabled – Displays whether or not the device is container-enabled.
Date/TimeDisplays the current time and time zone for the device, for example, UTC.
Summary
Network

This section displays information about the network settings, including DNS domain information and proxy settings.

Click Edit to set up the device, or to change the network configuration settings.

Time Service

Configure the time servers to which the device will synchronize its time.

Click Edit to configure the time service.

Enrollment InfoDisplays enrollment status for the device.
  • Enrolled – Status of device enrollment (yes, it is enrolled; no, it is not yet enrolled).
  • Enrollment Type
  • Edge Manager URL – If the enrollment type is certificate, the Predix Edge Manager certificate enrollment URL is displayed.
Network AdaptersDisplays information about the network LAN adapters, including MAC address, IP address, subnet mask, and default gateway.

Click Edit to configure the network and proxy settings.