Create an Enumerated Set
Procedure
- Access Configuration Hub.
- In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Tags.
-
Select
, and then select Manage Enumerated Sets.
The Manage Enumerated Sets: <system name> window appears. -
Select New Set, and enter values as described in the
following table.
The fields to create enumerated sets appear.
Field Description SET NAME Enter a name for the set. DESCRIPTION Enter a description for the set. DATA ATTRIBUTE ENUMERATED SET This is not applicable if you are creating an enumerated set. Set this to False. ENUMERATE BY Specify whether you want to define a single value or a range of values. A single value is best used with integer values because they match exactly. A range of values can be used with floating point values because they may not match exactly due to rounding.
NAME Enter a name for the state. VALUE Enter a numeric value for the state; string values such as on/off are not supported. This field appears only if you select Single Value in the ENUMERATE BY field. START RANGE and END RANGE Enter the start and end values of the range. Enter only numeric values; string values are not supported. These fields appear only if you select Range in the ENUMERATE BY field. If you want to assign ON for values 0-100, enter ON in the NAME field, and enter 0 and 100 in the START RANGE and END RANGE fields.
DESCRIPTION (under STATES) Enter a description for the state. - For each state that you want to create, select Add State, and repeat the previous steps.
- Select Save Set.
-
If needed, add more sets, and then select Done.
The enumerated set is created.