Registration with Configuration Hub for Webspace

After you install Webspace, you must launch the iFIX registration page to register it with the existing Configuration Hub server. Use these steps to register iFIX with Configuration Hub after Webspace is installed.

  1. On the machine where Webspace/iFIX is installed, click the Node Manager Configuration utility, as shown in the following figure.

    The following screen appears.

  2. Enter the Client ID and Client Secret you used for installing Proficy Authentication.
  3. Click Configure to register the node with Proficy Authentication.
  4. After registration is complete, refresh your web browser or logout and log back into the Configuration Hub.

    Result: After completing these steps for Configuration Hub, the Webspace panel should now work with the iFIX plugin.