Alarm Queue Configuration
Configuration Hub allows you to manage your iFIX alarm queue configuration from the Alarms panel.
Alarm Queue Overview
To access Alarm Queue Configuration:
- From the Navigation panel, select your node, iFIX project, and then Alarms.
- Click Configuration. The Alarm Queue settings appear as shown in the following figure.
Details of Alarm Queue Configuration
The following table displays the read-only fields of the Alarm Queue Configuration.
Field | Description |
---|---|
Service Name | The name of the Alarm service. |
Enabled | Whether the Alarm service is enabled or disabled. |
Size | The actual size of the service. The queue size is the number of records stored in the alarm queue. |
Min Size | The minimize size of the queue. This value can be any number from 1 to 32,767. |
Max Size | The maximum size of the queue. This value can be any number from 1 to 32,767.
The maximum queue size is the maximum number of records stored in the alarm queue. |
Last Modified User | The name of the user who last modified the service. |
Last Modified Time | The current time of the last modification. |
Version | The version of the queue. |