Getting Started with Operations Hub
This topic describes how to work with Operations Hub using the latest (HMI powered designer) and the classic version. For more complete details on how to use Operations Hub, refer to the Operations Hub help.
With 2023 release, Operations Hub is now available as a plug-in in Configuration Hub. The latest version is equipped with a HMI designer layout, and has enhanced plug-in functionality. All the features from the classic version of Operations Hub are also available in this latest version.
- Install the latest version of Operations Hub. Refer to Operations Hub and the Integrated Installer.
- Log in to the Operations Hub classic and set up the following:
- Data Sources (required)
- Queries
- Entities
- Themes (optional)
- Log in to the latest version of Operations Hub via Configuration Hub.
- Double-click the Configuration Hub desktop shortcut.
- Log in with the credentials that you specified during installation.
- On the Configuration Hub navigation panel, navigate to the Operations Hub home page. For more information on using the Operations Hub new layout, refer to Panels Layout.
- Create an application.
- Create pages for your application.
- Use the following features to design your application pages:
- Save the application pages, and preview the end application.