Line Connector
A line connector is a tool to show a connection between two or more objects.
Place two visual objects next to each other on a page, and draw a line connector to link them. You can draw straight line connectors or angle line connectors to link visual objects. You can use the line connector properties to:
- Customize line connector arrowheads to help explain the direction of the flow from one object to the other.
- Apply varied line styles.
- Add a unique color and thickness to the lines.
Draw Line Connector
To draw a line connector, follow these steps:
- On the page designer toolbar, select to activate the line connector.
- Single-click/mouse-click on the page where you want to draw.
- Start to draw the line by dragging the mouse in the direction you want the line to go. To add a vertex in line, single-click.
- To end the line connector, Shift-click. (On the keyboard, hold down the Shift key and release the mouse-click.)
- To deactivate the line connector, select on the page designer toolbar.
Add Vertex
A vertex is a node/point on the line connector. You can add a vertex on the line
connector to help demonstrate the relationships between multiple objects. To add a
vertex to any line connector:
- Select the line connector, for which you want to add a vertex.
- Double-click to select the area on the line connector where you want to add a vertex.
- Drag the vertex to create an angle.
Delete Line Connector
To delete a line connector:
- Select the line connector you want to delete.
- Select that appears next to the line connector. You can also select the Delete key on the keyboard to delete the line connector.
Line Connector Properties
Property | Description |
---|---|
Color | Use the color palette to apply a color to the line. |
Width | Enter a width to set the thickness of the line. |
Stroke Type | Define how you want the line to appear:
|
Start Marker End Marker |
Define a start/end line marker from these options:
|
Middle Marker | Define a line marker for the points in the middle of the line:
|
Layer | These layers are defined for line connectors so that they appear either
above or behind the plug-ins in the end application.
|
Rounded Corners | Select this check box if you want a round corner instead of a pointed corner. |