Workflow for Creating a Historian Model
Step Number | Description | Notes |
---|---|---|
1 | Set up Configuration Hub. | This step is required. It involves installing the required components to get started with Configuration Hub. |
2 | Create a collector instance. | This step is required. It involves creating a collector instance using which you want to collect data from the object instance and store it in an on-premises Historian server or a cloud destination. |
3 | Specify the tags for data collection. | This step is required. It involves specifying the tags for which
you want to collect data by browsing through the tags in the data
source. For example, for an iFIX collector, if there are 1,00,000
tags in the iFIX server, you must specify the ones for which you
want to collect data. Only then data is collected for those tags.
You will later map these tags with the variables in each object instance, thus collecting data for the variables (explained later in this workflow). |
4 | Create an object type. | This step is required. It involves creating an object type, a default template, one or more custom templates as needed, and adding variables to each object type. |
5 | Create an object instance. | This step is required. It involves creating an object instance and applying the required template from the object type. The object instance then inherits the variables from the object type. |
6 | Provide/collect data for static, direct, and indirect variables. | This step is required. You can provide data for the following
types of variables:
|