Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2023 releases, by signing up for one of our upcoming events.
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Model. Alternatively, you
can select Systems, and then in the row containing the
system in which you want to create a model, select , and then select
Browse Model.
The Model section appears.
Under Object Instances, right-click the object instance
that you want to delete (or select ), and then select
Delete.
A message appears, asking you to confirm that you want to delete the
object instance. If there are direct variables in the object type, you can also
choose to delete the tags associated with these variables (along with their
data).
Select Yes.
The object instance is deleted, along with the underlying variables and
templates.