Delete a Template

About this task

This topic describes how to delete a custom template. You cannot delete a template that is in use (that is, an object instance has been created for the object type). And, you cannot delete the default template in an object type.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Model. Alternatively, you can select Systems, and then in the row containing the system in which you want to create a model, select , and then select Browse Model.
    The Model section appears.
  3. In the main section, under Object Types, right-click the object type from which you want to delete a template (or select ), and then select Edit.
    The <object type name> section appears. The OBJECT TYPE TEMPLATE field contains the default template.
  4. In the OBJECT TYPE TEMAPLTE field, select the template that you want to delete.
  5. Next to the OBJECT TYPE TEMPLATE field, select, and then select Delete.
    A message appears, asking you to confirm that you want to delete the template.
  6. Select Yes.
    The template is deleted.
  7. In the upper-left corner of the page, select Save.
    The changes to the object type are saved.