Common Message Format Configuration
Configuration Hub allows you to manage your iFIX alarm message format from the Alarms panel.
Overview of Alarm Message Format Configuration
To access Alarm Message Format Configuration:
- From the Navigation panel, select your node, iFIX project, and then Alarms.
- Click Configuration and scroll to the Common Message Format section. The Common Message Format settings appear as shown in the following figure.
Details of Alarm Message Format Configuration
The following table describes the settings for the common message format fields.
Field | Description |
---|---|
Reset to Defaults button | Select this button to reset the settings back to the defaults. |
Date | The default is 10. |
Time | The default is 10. |
Node | The default is 10. |
Tagname | The default is 30. |
Alarm Type | The default is 7. |
Value | The default is 13. |
Unit | The default is 4. |
Message Length | The Message Length field allows you to specify the maximum number of characters that the printer can support. Valid entries are from 1-132. The default is 132. |
Current Length |
The Current Length field displays the number of characters that the printer currently supports. |