Navigation Panel
The Navigation panel contains the plugin instance of the name that you are currently logged into and the associated details. Examples are as follow:
- For Historian, the Navigation panel includes the Systems configured by user. Systems
will have Server details displayed. By default, there will be one system created. It
also includes the Model, Collectors, Tags, Data Stores, Archives, Data, Alarms, and
Activity Logs.
- In the case of iFIX, the plugin name is the node name of your iFIX node. Under
the node name, you will see a Default Project and Connections, Model, Database,
Webspace (if Webspace is installed and configured), HMI (if Operations Hub is
installed and configured), Project Security, Alarms, and Project Settings
panels.
- In the case of Operations Hub, you will see an Applications and Plugins panels.
Depending on the product, the Navigation panel will have different options available to open and configure.