Proficy Authentication Certificate

The location of the Proficy Authentication certificate is, by default:
C:\Program Files (x86)\Proficy\ConfigurationHub\UaaCert\uaa_cert.crt

During iFIX registration with Proficy Authentication, this certificate is automatically imported for you. However, if there is error or you want to reinstall the certificate, you can browse to the folder above on the installed product folder, and then copy it and register it manually.

Proficy Authentication Certificate

To install the Proficy Authentication certificate:

  1. Copy the uaa_cert.crt file from the C:\Program Files (x86)\Proficy\ConfigurationHub\UaaCert folder.
  2. Paste the uaa_cert.crt file to the destination computer.
  3. Double-click uaa_cert.crt to install the certificate. The Install Certificate screen appears.
  4. Click the Install Certificate button. The Import Certificate screen appears.
  5. Select Local Machine, and then Next. A message appears requesting if you want to proceed.
  6. Click Yes. The Certificate Store Screen appears.
  7. Select Place All Certificates in the Following Store.
  8. Click Browse, and then select Trusted Root Certificate Authorities and then click OK.
  9. Click Next. The final screen appears.
  10. Click Finish. A message should appear indicating the import was successful.
  11. Click OK.
  12. Restart the browser.