Configure iSCSI Initiator
This topic describes how to configure an iSCSI initiator and connect to the target server.
Before you begin
About this task
- A primary server called Node1
- A secondary server called Node2
Procedure
- Log in to the Node1 server.
- Go to .
- From the Server Manager dashboard, select .
-
Complete Add Roles and Features Wizard with these
options:
Section What To Do Before You Begin Skip to the next section. Installation Type Select Role-based or feature-based installation. Server Selection - Choose the option Select a server from the server pool.
- Under the server pool section, select your Node1 server. You will be installing the role/feature on this server.
Server Roles In the roles list box: - Expand .
- Select the check box for iSCSI Target Server.
Features To allow the installation of Failover Cluster Manager: - In the features list box, select the check box for
Failover Clustering.
The Add features that are required for Failover Clustering? screen appears, which shows the dependencies that are installed with this feature.
- Select Add Features.
Confirmation Select Install. The selected role and feature is installed on the Node1 server. - When the installation is complete, restart the machine.
- Log in to the same server again and launch Server Manager.
-
From the Tools menu, select iSCSI
Initiator.
- In the Target field, enter the iSCSI target server address.
-
Select Quick Connect.
If connected, the login success appears as shown in the following figure:
- Select Done, then OK to exit.
- Log in to the Node2 server and repeat steps 1-9.