Modify a Collector Instance
Note:
- If the status of a collector instance in unknown, you cannot modify it.
- You cannot modify the instance of an offline collector.
- Access Historian in Configuration Hub.
-
In the NAVIGATION section, select
Collectors.
A list of collectors appears.Tip: You can filter the collectors by the system name.
-
Select the collector instance that you want to modify.
The details of the collector appear in the DETAILS section.Tip: If the DETAILS section does not appear, in the upper-right corner of the page, select
, and then select Details.
-
As needed, modify values in the available fields.
Note: You cannot modify the destination of a collector.
-
In the upper-left corner of the page, select Save.The changes to the collector instance are saved.Note: For collectors earlier than version 9.0:
- You cannot modify the details in the INSTANCE CONFIGURATION section.
- Some of the details, such as the collector type, do not appear.
-
If a
icon appears next to the collector name in the main section, right-click the collector (or select
), and then select Restart.
The changes to the collector instance are saved.