Delete an Object Instance

  1. Access Configuration Hub.
  2. In the NAVIGATION section, select Model. Alternatively, you can select Systems, and then in the row containing the system in which you want to create a model, select , and then select Browse Model.
    The Model section appears.
  3. Under Object Instances, right-click the object instance that you want to delete (or select ), and then select Delete.
    A message appears, asking you to confirm that you want to delete the object instance. If there are direct variables in the object type, you can also choose to delete the tags associated with these variables (along with their data).
  4. Select Yes.
    The object instance is deleted, along with the underlying variables and templates.