Install Historian Administrator at a Command Prompt

Before you begin

Install Historian Administrator using the installer on a machine. When you do so, a template file named setup.iss is created at C:\Windows. This file stores the installation options that you have provided. You can then use this template to install Historian Administrator at a command prompt on other machines.

Procedure

  1. Copy the setup.iss file to the machine on which you want to install Historian Administrator at a command prompt.
  2. In the folder in which you have copied the file, run the following command: setup.exe /s /sms
    The installer runs through the installation steps.
    Note: If using certain versions of Windows (like Windows 10 or Windows 2019), you may receive an error message, stating that some of the DLL files are not registered. You can ignore these messages.
  3. When prompted to reboot your system, select Yes.

Results

Historian Administrator is installed.