Install Historian Administrator Using the Installer

About this task

If you already have Historian Administrator on your machine (installed using on-premises Proficy Historian), you can just change the destination to the NLB DNS, and begin using it:
  1. Select Main.

    A login window appears.

  2. Provide the NLB DNS, username, password, and domain information, and then select OK.

This topic describes how to install Historian Administrator using the installer. You can also install it at a command prompt.

Procedure

  1. Run the InstallLauncher.exe file. Contact the support team for this installer.
  2. Select Install Client Tools.
    The Select Features page appears, displaying a list of components.
  3. Select the Historian Administrator check box.
  4. Select Next.
    The Choose the Historian Program Folder page appears.
  5. As needed, change the destination folder of Historian Administrator, or leave the default folder, and then select Next.
    The Historian Server Name page appears.
  6. Enter the NLB DNS of Proficy Historian for AWS that you want to use with Historian Administrator, and then select Next.
    Tip: To find the NLB DNS:
    1. Access the EKS cluster on which you have deployed Proficy Historian for AWS.
    2. Access the EC2 instance.
    3. In the navigation pane, under Load Balancing, select Load Balancers.
    4. Select the load balancer for which you want to find the DNS.
    5. In the Description section, copy the DNS name.
  7. When you are asked to reboot your system, select Yes.