The Global Options Section
This topic describes the fields in each subsection in the Global Options section.
The Data Queries Subsection
Field | Description |
---|---|
Maximum Query Time (seconds) | Specifies the maximum time that a data point or query can take before it is terminated. Use this setting to limit query time and provide balanced read access to the archiver. This is applicable to all query types. |
Maximum Query Intervals | Specifies the maximum number of samples per tag that Historian can return from a non-raw data query. Use this setting to throttle query results for non-raw data queries. This setting is not applicable to filtered data queries or raw data queries. If the number of returned samples exceeds the value in this field, the query fails and no data is returned. |
The Memory/Recovery Subsection
Field | Description |
---|---|
Buffer Memory Max (MB) | The maximum memory buffer size that an archiver queue will use before starting to use disk buffering. The default value is 100 MB. Note:
|
Archiver Memory Size (MB) | The target memory usage of the archive. The default value is 0, which indicates the system will manage the memory usage. If the archiver is running on a 32-bit operating system and you want to keep more data in memory, you can enter a value up to 1800 MB. If the archiver is running on a 64-bit operating system, we recommend that you use the default value. |
Maintain Auto Recovery Files | Indicates whether high availability of the latest archive (.iha)
and Historian configuration (.ihc) files must be enabled. When
enabled, a copy of the latest .iha and .ihc file is made once every
hour. Note: These files are managed internally by Historian, and
should not be used as backup files. To create multiple archives
at the same time, select the Disabled
option. By default, this field is set to
Disabled on a 64-bit operating
system. On a large-scale system, we recommend that you disable
this option for better performance. |
The Data Store Subsection
Field | Description |
---|---|
Default Data Store For Tag Add | The name of the default data store to which you want to add tags. |