Install Local Help
When you install CIMPLICITY using the Proficy installer, the online help mode is selected by default. Pressing F1 in the application will direct you to the help on the GE Vernova documentation server. However, if you prefer to install the help locally, you can follow the steps provided in this topic.
Note: It is recommended to use the online help, as it is always updated.
To install the help locally,
- Ensure that projects are not running.
- Open Windows PowerShell as an administrator.
The Windows PowerShell prompt appears.
- In the PowerShell prompt, navigate to [ISO media
location]\CIMPLICITY\Setup\help.
For example, if the ISO media is in the D:\ drive, you can enter cd D:\CIMPLICITY\Setup\help.
- Execute the Setup.bat file by entering the .\Setup.bat command.
The help installation begins.
- After installing, in CIMPLICITY Options, change the help option to Local Help. For more information, refer to Configure Help.