Routes: Guidelines
- Item movement is directed from the Source Tracking Region to the Destination Tracking Region and cannot reverse direction along a single route.
- In a Tracking Route, if the Item Type is specified as a blank field or the wildcard character, all Types in the region are assumed to be allowed to travel this route between the Source and Destination Tracking Regions.
- The Item Type may also contain a mix of text and wildcard characters.
- The wildcard character is an asterisk (*).
- PRT determines what Item to move to a Destination Region by using these two rules.
If positive identification of the item (either ID or type) through information provided by the transition indicator:
Is made available to PRT | The item or item type identified is moved from the source region to the destination region. |
Not provided to PRT | The information PRT maintained about the Item(s) in the Source Region will be used. |