Unhighlight Event
Unhighlight triggers a procedure or calls a script after an object in CimView changes from highlight to not highlighted.

Field | Description | ||||
---|---|---|---|---|---|
A | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||
Procedure | |||||
Script | |||||
B | Parameter | Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Sub OnUnhighlight(highlightReason As Long) Where parameters are: | |||
highlightReason | |||||
C | Debounce event | Check | |||
Clear | |||||
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
|
Note: When the
Unhighlight
event is configured for an object, if the object is highlighted, a user can remove the highlight (unhighlight) the object by:- Removing the mouse cursor from it.
- Tabbing from it.
- Using arrow keys to leave it.