ActiveX Event

Note:  Each ActiveX control has its own set of events. See the documentation for the ActiveX control you plan to use.
Field Description
A ActiveX Event The drop-down list contains events that are available in the ActiveX control.
B Action Contains a drop-down list of existing procedures and scripts. Use either of the following.
Procedure  
Script  
C Parameter Available parameters depend on the selected ActiveX event. Can be used if the selected ActiveX event invokes a script. (The event can invoke a script directly or through a procedure.
D Debounce event Check  
Clear  
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.