Periodic Event
Periodic triggers a procedure or calls a script periodically at the rate you specify in the Time Period.

Field | Description | ||||||
---|---|---|---|---|---|---|---|
A | Time period | Number of milliseconds, seconds, minutes or hours between the time the event's procedure ends and the time it is re-triggered. | |||||
B | Time Type |
Select one of the following.
|
|||||
C | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||||
Procedure | |||||||
Script | |||||||
D | Parameter | These entry points have no parameters. | |||||
E | Debounce event | Check | |||||
Clear | |||||||
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start. This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory. |