Mouse Up Event
Mouse Up triggers a procedure or calls a script when the left mouse button is clicked then released.

Note: This event also occurs when a user releases the Enter key on the keyboard.
Field | Description | ||||||
---|---|---|---|---|---|---|---|
A | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||||
Procedure | ?? | ?? | ?? | ?? | |||
Script | ?? | ?? | ?? | ?? | |||
B | Parameter | Can be used if the event invokes a script directly or through a procedure parameters are: The default code begins as follows. Sub OnMouseUp(x As Long, y As Long, flags As Long) Where parameters are | |||||
x | ?? | ?? | ?? | ?? | ?? | ||
y | ?? | ?? | ?? | ?? | ?? | ||
?? | ?? | ?? | ?? | ?? | |||
flags | ?? | ?? | ?? | ?? | ?? | ||
?? | ?? | ?? | ?? | ?? | |||
?? | ?? | ?? | ?? | ?? | |||
?? | ?? | ?? | ?? | ?? | |||
C | Debounce event | Check | ?? | ?? | ?? | ?? | ?? |
Clear | ?? | ?? | ?? | ?? | ?? | ||
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
|