Object Shadow
Shadows can help give objects a 3-D effect and make them stand out on a CimView screen.
CimEdit options provide you with the flexibility to create normal or diffuse shadows at selected distances and angles in custom selected transparent or opaque colors.
1 | Display shadow properties. |
2 | Select shadow properties. |
Display Shadow Properties
- Select the object that will have the shadow.
- Do one of the following.
- Double-click the object
- Right-click the object; select Properties on the Popup menu.
- Click the Properties button in the Home>Properties group.
Result: The object's Properties dialog box opens.
Select Shadow Properties
Select Shadows in the Properties dialog box.
Shadows specifications are as follows.
A | Style |
B | Distance |
C | Angle |
D | Color |
A | Style |
The shadow style provides a solid or more blurred effect.
Shadow style options are:
Option | The shadow attribute: |
None | Is not applied to the object. Note: If the object included a shadow when it was inserted, that shadow will continue to display. |
Normal | Includes all of the pixels assigned to the selected color transparency, giving the shadow a more solid appearance. |
Diffuse | Presents a gradient type, blurred view. |
B | Distance |
The entered distance causes the shadow to:
- Move closer to or away from the object.
- Be more or less prominent.
- Influence the 3-D effect.
Note: The distance is tied to the angle, which determines where the shadow will be placed relative to the object.
Example
The shadow display for an object with a diffuse 50% transparent black (at a 315 degree (-45 degree) angle) depends on its specified distance.
Distance | Shadow Display |
5 Pt. | When the shadow distance is small, the shadow is almost hidden. |
10 Pt. | As the shadow distance increases, the shadow becomes more noticeable. |
15 Pt. | A higher shadow distance continues to make the shadow more noticeable. |
C | Angle |
The angle influences the object's perspective.
0?? | 45?? | 90?? | 135?? |
180?? | |||
360??/0?? | 315??/-45?? | 270??/-90?? | 225??/135?? |
D | Color |
The shadow can be any color at any transparency.
Example