Family Field Descriptions

Family Field Descriptions

This topic provides a listing of all the families in the Rounds Designer module, with links to the family fields information.

Checkpoint Condition Records

Checkpoint Condition records store details about the conditions of Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Checkpoint Condition family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

Note: We do not recommend modifying Checkpoint Condition records outside of the Rounds Designer module. This may cause unexpected results with an existing Route that is currently using that condition.

Field

Data Type

Description

Behavior and Usage

Condition IDCharacterA unique value that identifies the condition of the CheckpointThis field is populated automatically by the Rounds module. Alternatively, you can enter a value in this field, but the value must be unique.
Field NameCharacterThe name of the Checkpoint conditionThis field is populated automatically by the template or by the data loader used to create the condition, or by the Rounds Designer module.
Field Value for Character TypeCharacterThe field that stores the value of the Checkpoint condition if the value is a character valueThe use of this field as opposed to the Field Value for Numeric Type field is determined by the predecessor Checkpoint record of the Condition record.

You can enter the value of this field in the Select Value box when adding a condition to a Checkpoint.

Field Value for Numeric TypeNumericThe field that stores the value of the Checkpoint condition if the value is a numeric valueThe use of this field as opposed to the Field Value for Character Type field is determined by the predecessor Checkpoint record of the Condition record.

You can enter the value of this field in the Select Value box when adding a condition to a Checkpoint.

Possible ConditionCharacterThe relational value of a CheckpointYou can select the value of this field in the Select Relation box when adding a condition to a Checkpoint.
Predecessor KeyNumericThe entity key of a predecessor CheckpointThis field is populated automatically by the predecessor Checkpoint.
Related Template Group KeyNumericThe entity key of the Template Group applied to the Route containing the Checkpoint conditionThis field is populated automatically by the Template Group key that generated the condition.
Route KeyNumericThe entity key of the Route containing the Checkpoint conditionThis field is populated automatically by the Route of which the condition is a part.
TypeCharacterThe type of Checkpoint conditionThis field is populated by the predecessor Checkpoint record of the Condition record.

Checkpoint Task Records

Checkpoint Task records store details on the schedule on which a Checkpoint should be executed. This topic provides an alphabetical list and description of the fields that exist for the Checkpoint Task family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Last DateDateThe date on and time at which the last reading was recorded for this CheckpointThis field is populated automatically after a Reading is created and linked to the Measurement Location to which the Checkpoint Task is linked, with the value in the Reading Taken Date field of the Reading.
Next DateDateThe date on and time at which the next reading for this Checkpoint becomes dueThis field is populated automatically based on the values in the Schedule field and the Last Date field. If the Last Date field is empty, the value in the Next Date field is calculated as the next date and time that meets the defined schedule after the current date and time.
Non-compliance DateDateThe date and time after which the reading will be considered non-compliant

This field is populated automatically based on the values in the Schedule and the Next Date fields.

By Default, Non-Compliance Date value is populated as: Next Date Value + Non Compliance Date Interval (in days). If Non Compliance Date Interval is absent, then Next Compliance Date value is populated as: Next Date + Schedule Interval.

Non-Complinace Date IntervalNumericThe Non Compliance Date Interval (in days) added to Next Date to get the Non-Compliance Date

This field is not populated automatically.

If Non Compliance Date Interval is absent, then Next Compliance Date value is populated as: Next Date + Schedule Interval.

Non-Compliance Next Check DateDateThe date after which the Checkpoint is checked again for Compliance

By Default, Non-Compliance Next Check Date value is = Non-Compliance Date

ScheduleCharacterThe schedule by which you want to take readings for this Checkpoint.This field contains an ellipsis button that you can select to access the Edit Schedule window, where you can define the schedule for the associated Checkpoint.
Task IDCharacterThe ID of the Checkpoint TaskThis field is populated automatically with a value in the format CP-<n>, where <n> is a number representing the number of Checkpoint Tasks that have been initiated (even if they were not actually saved). You can change the value, if needed.

Checkpoint Template Records

Checkpoint Template records store details about Checkpoint templates that can be used to create Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Checkpoint Template family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Automatically create health indicatorBooleanIndicates whether a health indicator will be created automaticallyIn the datasheet, this field appears as a check box labeled Automatically create health indicator. When selected, a health indicator will be created automatically when the Checkpoint is created.
Checkpoint LockedBooleanIndicates whether or not a Checkpoint will be locked until the device user scans the associated barcodeIn the datasheet, this field appears as the Scan to Unlock? check box.

When this field is set to:

  • True, the device user must scan the barcode associated with a Checkpoint that was created from the Checkpoint template before recording readings.
  • False, the device user does not have to scan the barcode associated with a Checkpoint that was created from the Checkpoint template before recording readings.
Note:
  • This feature is not available on tablet devices.
  • The Scan to Unlock functionality is currently activated in the following versions:
    • 4.5.0.0.0
    • 4.3.0.7.x with patch 10 activated in the release
Content GUID CharCharacterCharacter value of system field Content GUIDYou can use this field to create a query that links a Checkpoint to its related Checkpoint template.
DescriptionCharacterA description of the templateIn this box, you can enter a description of the action users will be completing when they enter readings for this Checkpoint.
Include as Health Indicator SourceBooleanIndicates whether a potential health indicator source is used to create health indicators.In the datasheet, this field appears as a check box labeled Include as Health Indicator Source. When this check box is selected, health indicators are created for the selected source. When the check box is cleared, health indicators are not created for the selected source.
Non Compliance Date IntervalNumericThe number of days without a reading before the Checkpoint is considered non-compliantYou can enter a positive integer in this field.

If the Non Compliance Date Interval field is blank, the Next Compliance Date value is populated with the combined values of the Next Date field in the Checkpoint Task family and the Schedule Interval, which is part of the Schedule field in the Checkpoint Task family.

Requires Equipment ShutdownBooleanIndicates whether or not the equipment requires shutdownIn the datasheet, this field appears as a check box, which is cleared by default.
ScheduleCharacterThe schedule by which you want to take readings for the Checkpoint templateYou can select to view the Schedule window, where you can define the schedule for the Checkpoint template.
StatusCharacterThe status of the CheckpointIn the datasheet, this field appears as a list that is populated by the MI_FDC_STATUS_TYPE System Code Table. It is labeled Status and contains the following values:
  • Active
  • Inactive
You can select a value from the list.

The value in this field is set to Active by default.

Inactive Checkpoints will not appear in the Data Collection page.

Template IDCharacterThe ID for the templateA value is required and must be unique. If you enter a value that is not unique to the Checkpoint template, a message appears indicating that the ID already exists.
Unit of MeasureCharacterThe unit of measure that users can specify when entering a numeric reading value for the CheckpointThis field appears as a list that is populated by the UOME System Code Table.

This field is disabled if the value in the ML Type field in the Measurement Location family is set to Character, or if the value in the LR Type field in the Lubrication Requirement family is set to Check Off.

Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Measurement Location contains all the values from the UOME system code table, sorted by their descriptions.

The UOM field for a Lubrication Requirement contains a subset of values from the UOME system code table based on specific reference values from the MI_LM_REFERENCES system code table.

Lubricant Records

This topic provides an alphabetical list and description of the fields that exist for the Lubricant family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

Lubricant records serve as a means for organizing all the lubricants that are used by your company. When you create a Lubricant record, the values that you enter in these fields will be used to populate the corresponding lists on the Lubrication Requirement datasheet, where you can select the necessary values from a list.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Description CharacterDescription of the lubricantYou can enter a value in this field.
Flash Point NumericFlash point of the lubricantYou can enter a value in this field.
Flash Point UOMCharacterThe unit of measurement of the Flash point of the lubricantOn the datasheet, this field appears as a list that is populated by the MI_LUBRICANT_REFERENCES system code table.
Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Lubrication Requirement contains a subset of values from the UOME system code table based on specific reference values from the MI_LM_REFERENCES system code table.

ISO Grade CharacterViscosity grading of the lubricantYou can enter a value in this field.
Lubricant CharacterThe name of the lubricantYou can enter a value in this field.
Lubricant Type CharacterThe type of lubricantOn the datasheet, this field appears as a list that is populated by the MI_LUBR_TYPE system code table.
Manufacturer NumericThe manufacturer of the lubricant

On the datasheet, this field appears as a list that is populated with the values stored in the Manufacturer Name field in existing Lubricant Manufacturer records.

This field displays the Manufacturer Name, but stores the Entity Key of the corresponding Lubricant Manufacturer record.

If you are creating multiple Lubricant records, you may select the same or different manufacturers for each.

Manufacturer's Part NumberCharacterManufacturer part number of the lubricantYou can enter a value in this field.
Material NumberCharacterMaterial number of the Lubricant (for example, the material number used in your EAM system)You can enter a value in this field.
NotesCharacterAny notes necessary for the lubricantYou can enter a value in this field.
Storage LocationCharacterLocation where the lubricant is storedYou can enter a value in this field.
Trade NameCharacterBrand name of the lubricantYou can enter a value in this field.
Viscosity RatingCharacterViscosity index of the lubricantYou can enter a value in this field.

Lubricant Manufacturer Records

Lubricant Manufacturer records store details about the manufacturer of a lubricant. This topic provides an alphabetical list and description of the fields that exist for the Lubricant Manufacturer family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Manufacturer IDCharacterThe ID that you want to use to identify a lubricant manufacturerThis field is required and must be unique.
Manufacturer NameCharacterThe name of a lubricant manufacturer

This field is required and must be unique.

This field is used to populate the list in the Manufacturer field of Lubricant records.

Manufacturer DescriptionCharacterA description of the lubricant manufacturerThis field is optional.

Lubrication Component Records

Lubrication Component records store information about lubrication components and provide values for drop-down lists used in the Lubrication Requirement and Lubrication Requirement Template families. This topic provides an alphabetical list and description of the fields that exist for the Lubrication Component family and appear on the Lubrication Component datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Component Sub TypeCharacterThe sub type of a lubrication component typeThe values in this field populate the Component Sub-Type lists on Lubrication Requirement and Lubrication Requirement Template datasheets.
Component TypeCharacterThe type of lubrication component

Organizes records in the Lubrication Component family into distinct groups.

The values in this field populate the Component lists on Lubrication Requirement and Lubrication Requirement Template datasheets.

DescriptionCharacterThe description of the lubrication component type or sub typeIf there is a value in the corresponding Component Sub Type field, then the value in this field is a description of the Component Sub Type. However, if the corresponding Component Sub Type field is empty, then the value in this field is a description of the Component Type.
IDCharacterA unique value that identifies the lubrication componentThis field is required and must be unique.

Lubrication Management Recommendation Record

This topic provides an alphabetical list and description of the fields that exist for the Lubrication Management Recommendations. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Asset IDNumericThe ID of the Asset for which the recommendation is being madeThis is Unique for a particular equipment.
Assigned To NameTextName of the person responsible for ensuring the recommendation is implementedEnter the name of the person to whom would be responsible for ensuring the recommendation is implemented.
Author Name TextName of the person proposing the recommendationYou can enter the name of the user to which the recommendation is associated.
Create Work Request?Check boxEnables a work requestAll the other Work request details are enabled after the check box is selected.
Final Approver NameTextName of the individual ultimately responsible for approving the recommendation and the associated expenditureYou can pick a user from the list as an approver.
Recommendation BasisTextThe background as to why the recommendation is being madeYou can type in the description in the text box.
Recommendation DescriptionTextDetails of the recommendationYou can type in the description in the text box.
Recommendation HeadlineTextA brief summary of the recommendation subjectDisabled after the author has set the author lock.
Recommendation IDTextThe unique ID for the RecommendationThis is unique.
Recommendation PriorityPicklistThe priority of recommendation for implementation

Enter the value from the list that best represents the priority of recommendation for implementation.

  • High
  • Medium
  • Low
 
Required Equipment StatusCharacterThe operating state the Equipment or Functional Location needs to be in, in order to implement the recommendationNone
Reviewer NameTextName of the individual responsible for reviewing and endorsing the recommendationYou can pick a user as a reviewer from the list.
Target Completion DateDateDate by which the recommendation is intended to be implementedUser to select a date from the calendar.
Technical NumberNumericNumber associated with the equipment and recommendation requestThis number is unique.
Work Request EquipmentCharacterThe work request associated with EquipmentThis is populated automatically.
Work Request Functional Location CharacterThe work request associated with the Functional Location recordThis is populated automatically.
Work Request ReferenceNumericThe ID of the work request that may be associated with the recommendationThis is populated automatically.

Lubrication Requirement Records

Lubrication Requirement records store details about Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Lubrication Requirements family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Asset DescriptionCharacterA description of the equipment or location represented by the Equipment or Functional Location to which you want to link the Lubrication Requirement

On the datasheet, this field appears as a text box labeled Asset Description.

When the Lubrication Requirement is linked to:

  • An Equipment, this field is populated automatically with the value in the Equipment Short Description field in the linked Equipment.
  • A Functional Location, this field is populated automatically with the value in the Functional Location Description field in the linked Functional Location.

If you do not want GE Digital APM to populate the field automatically, you can enter a description for the equipment or location directly into the Asset Description cell.

Asset IDCharacterThe ID of the Equipment or Functional Location to which you want to link the Lubrication Requirement

On the datasheet, this field appears as a text box labeled Asset ID.

When the Lubrication Requirement is linked to:

  • An Equipment, this field is populated automatically with the value in the Equipment ID field in the linked Equipment.
  • A Functional Location, this field is populated automatically with the value in the Functional Location field in the linked Functional Location.
CapacityNumberA number representing the amount of lubricant that the component will holdYou can enter a value in this field.
Capacity Unit of MeasureCharacterA value representing the UOM associated with the value in the Capacity fieldOn the datasheet, this field appears as list that is populated by the MI_LM_REFERENCES system code table.
Checkpoint IDCharacterThe ID of the Checkpoint for the Lubrication RequirementYou can enter a value in this field.
Component Sub TypeCharacterThe subtype of a lubrication component type

On the datasheet, this field appears as a list labeled Component Subtype and is populated with the values stored in the Component Sub Type field in the existing Lubrication Component records.

This list is filtered by the value that you select in the Component list.

Component TypeCharacterThe type of lubrication componentOn the datasheet, this field appears as a list labeled Component and is populated with the values stored in the Component Type field in the existing Lubrication Component records.
DescriptionCharacterA description of the Checkpoint

On the datasheet, this field appears as a text box labeled LR Description.

In this box, you can enter a description of the action users will be completing when they enter readings for this Checkpoint.

This is a required field.

LR TypeCharacterThe type of data that users can enter when creating a Reading linked to the Lubrication RequirementOn the datasheet, this field appears as a list that is populated by the MI_LM_LUBR_REQ_TYPE system code table.
LubricantCharacterThe lubricant that is required for this Checkpoint

On the datasheet, this field appears as a list labeled Lubricant and is populated with the values stored in the Lubricant field in the existing Lubricant records.

This list is filtered by the values that you select in the Lubricant Manufacturer and Lubricant Type lists.

Lubricant ManufacturerCharacterThe company that manufactures the lubricant that users should use when completing this Checkpoint

On the datasheet, this field appears as a list labeled Lubricant Manufacturer and is populated with the values stored in the Lubricant Manufacturer field in the existing Lubricant records.

This list is filtered by the values that you select in the Lubricant list. If you have not yet selected a lubricant, the list is filtered based on the possible lubricants that you could select.

Lubricant TypeCharacterThe type of LubricantOn the datasheet, this field appears as a list that is populated by the MI_LUBR_TYPE system code table.
Method Sub TypeCharacterThe subtype of a lubrication method type

On the datasheet, this field appears as a list labeled Method Sub Type and is populated with the values stored in the Sub Type field in the existing Lubrication Method records.

This list is filtered by the values that you select in the Lubricant and Method Type lists.

Method TypeCharacterThe method by which the lubricant must be applied

On the datasheet, this field appears as a list labeled Method Type and is populated with the values stored in the Type field in the existing Lubrication Method records.

This list is filtered by the value that you select in the Lubricant list.

Number of PointsCharacterThe number of points on the component that requires lubricationYou can enter the number of points that require lubrication. For example, if the component is an axle, you might enter 2 in this field.
PriorityCharacterA value representing the priority associated with the lubrication requirementOn the datasheet, this field appears as a list that is populated by the MI_LUBR_PRIORITY system code table.
Related Ref Doc Image KeyNumericThe entity key of a reference documentOn the datasheet, this field appears as a text box labeled Checkpoint Image in which you can enter or select a reference document image that will be downloaded to a device and displayed when you access a checkpoint in Rounds Data Collection.
Requires Equipment ShutdownBooleanIndicates whether the equipment requires shutdownOn the datasheet, this field appears as a check box, which is cleared by default.
StatusCharacterThe status of the Lubrication Requirement

On the datasheet, this field appears as a list labeled Status and contains the following values:

  • Active
  • Inactive

This field contains the value Active by default.

Inactive Lubrication Requirement records will not appear in Data Collection pages.

TemplateCharacterThe Lubrication Requirement Template that you want to use to populate fields in the Lubrication Requirement

On the datasheet, this field appears as a list displaying the Template IDs of the Lubrication Requirement Template records in your database. When you select a value, other fields in the record will be populated automatically based on the values in that template.

After you save a Lubrication Requirement, the Content GUID of the selected Lubrication Requirement Template record is stored in the Template field, and the field is disabled.

Unit of MeasureCharacterThe unit of measure that you can specify when entering a numeric reading value for a CheckpointOn the datasheet, this field appears as a list that is populated by the MI_LM_REFERENCES system code table. This field is disabled if the value in the LR Type field is Check Off.
Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Lubrication Requirement contains a subset of values from the UOME system code table based on specific reference values from the MI_LM_REFERENCES system code table.

Lubrication Requirement Template Records

Lubrication Requirement Template records can be used to create Lubrication Requirement records and contain all the fields included in Lubrication Requirement records, with the exception of the Template field in the Lubrication Requirement record. In addition, Lubrication Requirement Template records include the additional field Template ID, which stores the ID for the template. This value appears in the Template field in the Lubrication Requirement record.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

Measurement Location Records

Measurement Location records store details about Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Measurement Location family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Allowable ValuesCharacterThe values the user can select when entering a reading for this CheckpointOn the datasheet, this field appears as a list labeled Allowable Values and contains all the values in the Value field in the Operator Rounds Allowable Values family whose type values match the value stored in the ML Type and Category lists in the Measurement Location. To select or clear the field, select the value in the list. The indication that a value is selected is the vertical blue line to the left of the value.

For example, suppose you select Character in the ML Type list and Pump Check in the Category list in a Measurement Location. If four allowable values contain the value Character in their Type field and Pump Check in their Category field, the Allowable Values list on the Measurement Location datasheet will contain the values in the Value field of those four allowable values.

The values in this list are also used to populate the Numeric and Character lists on the Limit Values section of the ML Task View datasheet. These values are used to set up alerts that will be displayed to device users if they enter a certain reading value.

In the Action section of the ML datasheet, the user can add Action Taken values to a list for any Measurement Location separately for the Limit Values.

If you clear a check box from the Allowable Values list and the corresponding allowable value is used in the Limit Values section, that allowable value will automatically be removed from the Limit Values section.

Allowable Values TempCharacterTemporary field used by family policies to store values as they are being updatedBy default, this field does not appear on the datasheet, and users cannot enter values into this field. The field is latent unless the Before Update and After Update Family Policies in the Operator Rounds Allowable Values family are activated. If these family policies are activated, this field temporarily stores Allowable Value changes during an update.
AssetCharacterThe Equipment or Functional Location which the user can add for the MLOn the datasheet, you can link an Equipment or a Functional Location to the Measurement Location. Depending on the selection, the Asset field is populated automatically. Also, the Asset Description, Asset ID fields are also populated.
Asset DescriptionCharacterA description of the equipment or location represented by the Equipment or Functional Location to which you want to link the Measurement LocationWhen the Measurement Location is linked to:
  • An Equipment, this field is populated automatically with the value in the Equipment Short Description field in the linked Equipment.
  • A Functional Location, this field is populated automatically with the value in the Functional Location Description field in the linked Functional Location.

If you do not want GE Digital APM to populate the field automatically, you can enter a description for the equipment or location directly into the Asset Description cell.

Asset IDCharacterAn ID of the equipment or location represented by the Equipment or Functional Location to which you want to link the Measurement LocationThis field is populated automatically.
Automatically create health indicatorBooleanIndicates whether a health indicator will be created automaticallyIn the datasheet, this field appears as a check box labeled Automatically create health indicator. When selected, a health indicator will be created automatically when the Checkpoint is created.
CategoryCharacterThe category to which the Checkpoint belongsOn the datasheet, this field appears as a list labeled Category and contains the values that are defined in the Category field in the Operator Rounds Allowable Values family whose type matches the value that is stored in the ML Type field in the Measurement Location. You can select a value from the list.

For example, if you select Character in the ML Type list in a Measurement Location and four allowable values contain the value Character in their Type fields, the Category list on the Measurement Location datasheet will contain the values in the Category field of those four allowable values.

Category TempCharacterTemporary field used by family policies to store values as they are being updatedBy default, this field does not appear on the datasheet, and users cannot enter values into this field. The field is latent unless the Before Update and After Update Family Policies in the Operator Rounds Allowable Values family are activated. If these family policies are activated, this field temporarily stores Category changes during an update.
Checkpoint IDCharacterThe ID of the Checkpoint for the Measurement LocationYou can enter a value in this field.
Checkpoint LockedBooleanIndicates whether a Checkpoint should be locked on the Windows Mobile Device until the device user scans the associated barcodeOn the datasheet, this field appears as a check box labeled Scan to Unlock?.

When this field is set to:

  • True, the device user must scan the barcode associated with a Measurement Location before recording readings.
  • False, the device user does not have to scan the barcode associated with a Measurement Location before recording readings.

This field is disabled when the Scan ID field is disabled.

Note: This feature is not supported on tablet devices.
DescriptionCharacterA description of the CheckpointOn the datasheet, this field appears as a text box labeled ML Description.

In this box, you can enter a description of the action users will be completing when they enter readings for this Checkpoint (e.g., Pump Check, Vibration Check, or Temperature Check).

This is a required field.

Download Stored DocumentBooleanIndicates whether the Reference Documents associated with a route will be downloaded to a Windows CE mobile deviceOn the datasheet, this field appears as a check box.

By default, this field is set to:

  • False, when the combined file size of the associated reference document files is greater than 2 MB. When this field is set to False, the associated files will not be downloaded to the device.
  • True, when the combined file size of the associated reference document files is less than or equal to 2 MB. When this field is set to True, the associated files will be downloaded to the device.
Note: Document download is not supported on tablet devices. However, tablet devices can open document types, regardless of file size, when connected to the GE Digital APM Server.
Equipment Technical NumberCharacterThe Equipment Technical Number of the EquipmentOn the datasheet, this field appears as a text box labeled Equipment Technical Number. If the Measurement Location is linked to an Equipment, this field is populated automatically with the value stored in the Equipment Technical Number field in the Equipment.
Include as Health Indicator SourceBooleanIndicates whether a potential health indicator source is used to create health indicators.In the datasheet, this field appears as a check box labeled Include as Health Indicator Source. When this check box is selected, health indicators are created for the selected source. When the check box is cleared, health indicators are not created for the selected source.
Maximum Target ValueNumericA number representing the highest target reading value that is acceptable for the CheckpointOn the datasheet, this field appears as a text box labeled Maximum Target Value, in which you can enter a number. Together, the value stored in this field and the value stored in the Minimum Target Value field define a target range that appearson the More Information screen on a Windows Mobile device.
Note: This feature is not supported on tablet devices.

This field is disabled when the value in the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Target Value field with the value you enter in the Minimum Target Value field. If you enter a value in the Maximum Target Value field that is less than the value in the Minimum Target Value field, a message will appear, indicating that the value must be greater than the value in the Minimum Target Value.

Maximum Valid ValueNumericA number representing the highest reading value that is acceptable for the CheckpointOn the datasheet, this field appears as a text box labeled Maximum Valid Value, in which you can enter a number. This value is used by the mobile device to check the reading value that is entered by the device user and display a message if the value they enter is higher than this value. Together, this value and the value in the Minimum Valid Value field define the valid value parameters for a reading.
Note: This feature is not supported on tablet devices.

This field is disabled when the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Valid Value field with the value you enter in the Minimum Valid Value field. If you enter a value in the Maximum Valid Value field that is less than the value in the Minimum Valid Value field, a message will appear, indicating that the value must be greater than the value in the Minimum Valid Value.

Minimum Target ValueNumericA number representing the lowest target reading value that is acceptable for the Checkpoint

On the datasheet, this field appears as a text box labeled Minimum Target Value, in which you can enter a number. Together, the value stored in this field and the value stored in the Maximum Target Value field define a target range that appearson the More Information screen on the mobile device.

Note: This feature is not supported on tablet devices.

This field is disabled when the value in the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Target Value field with the value you enter in the Minimum Target Value field. If you enter a value in the Minimum Target Value field that is greater than the value in the Maximum Target Value field, a message will appear, indicating that the value must be less than the value in the Maximum Target Value.

Minimum Valid ValueNumericA number representing the lowest reading value that is acceptable for the CheckpointOn the datasheet, this field appears as a text box labeled Minimum Valid Value, in which you can enter a number. This value is used by the mobile device to check the reading value that is entered by the device user and display a message if the value they enter is lower than this value. Together, this value and the value in the Maximum Valid Value field define the valid reading value parameters for a Checkpoint.
Note: This feature is not supported on tablet devices.

This field is disabled when the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Valid Value field with the value you enter in the Minimum Valid Value field. If you enter a value in the Minimum Valid Value field that is greater than the value in the Maximum Valid Value field, a message will appear, indicating that the value must be less than the value in the Maximum Valid Value.

ML TypeCharacterThe type of data that users can enter when creating a Reading linked to the Measurement LocationOn the datasheet, this field appears as a list labeled ML Type and contains the following values:
  • Character. If you select Character, users can record any reading value for this Checkpoint.
  • Numeric. If you select Numeric, they must record a numeric reading value for this Checkpoint.
More InformationCharacterAdditional instructions about the Checkpoint that you want to be displayed on the Data Collection pageThis field appears on the Data Collection page and is labeled Additional Instructions on that page.
ProductCharacterThe product produced by the piece of equipment that is associated with this CheckpointOn the datasheet, this field appears as a cell. You can enter a value directly in the Product cell.

You can use this field to differentiate which Checkpoint is relevant depending on the current product for equipment that is used to produce multiple products. The field would be used as a filter in a customized download query to include only the relevant Checkpoints depending on the current product. This feature is only supported for Windows CE mobile devices that use a customizable download query.

Note: This feature is not supported on tablet devices.
Related Asset IdCharacterThe ID of the Equipment or Functional Location to which you want to link the Measurement LocationOn the datasheet, this field appears as a text box labeled Asset ID.

When the Measurement Location is linked to:

  • An Equipment, this field is populated automatically with the value in the Equipment ID field in the linked Equipment.
  • A Functional Location, this field is populated automatically with the value in the Functional Location field in the linked Functional Location.
Related Ref Doc Image KeyNumericThe entity key of a reference documentOn the datasheet, this field appears as a text box labeled Checkpoint Image in which you can enter or select a reference document image that will be downloaded to a device and displayed when you access a checkpoint in Rounds Data Collection.
Requires Equipment ShutdownLogicalIndicates whether the equipment requires shutdownOn the datasheet, this field appears as a check box, which is cleared by default.
Scan IDCharacterThe ID of the barcode that identifies the CheckpointThis field is enabled only when you are working with a Measurement Location that is linked directly to a Route, (i.e., it is disabled when you are working with a Measurement Location that is linked to a predecessor Checkpoint Condition).

If you have assigned a Scan ID to the Equipment or Functional Location linked to the Measurement Location, the Scan ID field on the Measurement Location datasheet will be populated with the same Scan ID that appears in the Equipment or Functional Location.

StatusCharacterThe status of the Measurement LocationOn the datasheet, this field appears as a list labeled Status and contains the following values:
  • Active
  • Inactive

You can select a value from the list. This field contains the value Active by default.

Inactive Measurement Locations will not appear on Data Collection pages.

TemplateCharacterThe Measurement Location Template that you want to use to populate fields in the Measurement LocationOn the datasheet, this field appears as a list displaying the Template IDs of the Measurement Location Template records in your database. When you select a value, other fields in the record will be populated automatically based on the values in that template.

After you save a Measurement Location, the Content GUID of the selected Measurement Location Template record is stored in the Template field, and the field is disabled.

Unit of MeasureCharacterThe unit of measure that users can specify when entering a numeric reading value for the CheckpointOn the datasheet, this field appears as a list labeled Unit of Measure. You can select a value from the list. This field is disabled if the ML Type field contains the value Character.
Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Measurement Location contains all the values from the UOME system code table, sorted by their descriptions.

Measurement Location Template Records

Measurement Location Template records store details about measurement location templates that can be used to create Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Measurement Location Template family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

Note: For more information on Measurement Location Template family fields, refer to the reference information for the matching fields in the Measurement Location family.
FieldData TypeDescriptionBehavior and Usage
Allowable ValuesCharacterThe values the user can select when entering a reading for the Checkpoint created from the templateOn the datasheet, this field appears as a list labeled Allowable Values and contains all the values in the Value field in the Operator Rounds Allowable Values family whose type and category values match the values stored in the ML Type and Category lists in the Measurement Location Template. You can select values in this list to indicate that the corresponding allowable value should appear on the device for a Checkpoint created from the template.

For example, suppose you select Character in the ML Type list and Pump Check in the Category list in a Measurement Location Template. If four allowable values contain the value Character in their Type fields and Pump Check in their Category fields, the Allowable Values list on the Measurement Location Template datasheet will contain the values in the Value fields of those four allowable values.

The values in this list are also used to populate the Numeric and Character lists on the Limit Values section of the ML Task View datasheet. These values are used to set up alerts that will be displayed to device users if they enter a certain reading value.

On the Action section of the ML datasheet, the user can add Action Taken values to a list for any Measurement Location Template separately for the Limit Values.

Allowable Values TempCharacterTemporary field used by family policies to store values as they are being updatedBy default, this field does not appear on the datasheet, and users cannot enter values into this field. The field is latent unless the Before Update and After Update Family Policies in the Operator Rounds Allowable Values family are activated. If these family policies are activated, this field temporarily stores Allowable Value changes during an update.
CategoryCharacterThe category to which the Checkpoint belongsOn the datasheet, this field appears as a list labeled Category and contains the values that are defined in the Category field in the Operator Rounds Allowable Values family whose type matches the value that is stored in the ML Type field in the Measurement Location. You can select a value from the list.

For example, if you select Character in the ML Type list in a Measurement Location and four allowable values contain the value Character in their Type fields, the Category list on the Measurement Location datasheet will contain the values in the Category field of those four allowable values.

Category TempCharacterTemporary field used by family policies to store values as they are being updatedBy default, this field does not appear on the datasheet, and users cannot enter values into this field. The field is latent unless the Before Update and After Update Family Policies in the Operator Rounds Allowable Values family are activated. If these family policies are activated, this field temporarily stores Category changes during an update.
Checkpoint LockedBooleanIndicates whether a Checkpoint will be locked on a Windows Mobile Device until the device user scans the associated barcode

On the datasheet, this field appears as a check box labeled Scan to Unlock?.

On the datasheet, this field appears as a check box labeled Scan to Unlock?. This field is populated automatically in new Measurement Locations that are created from the Measurement Location Template. If you modify this value, it is not updated automatically in Measurement Locations that were created from the Measurement Location Template. When this field is set to:

  • True, the device user must scan the barcode associated with a Measurement Location that was created from the Measurement Location Template before recording readings.
  • False, the device user does not have to scan the barcode associated with a Measurement Location that was created from the Measurement Location Template before recording readings.
Note:
  • This feature is not available on tablet devices.
  • The Scan to Unlock functionality is currently activated in the following versions:
    • 4.5.0.0.0
    • 4.3.0.7.x with patch 10 activated in the release
Content Guid CharCharacterCharacter value of system field Content GUID

You can use this field to create a query that links a Checkpoint to its related Checkpoint template.

This field is inherited from the Checkpoint Template family.

DescriptionCharacterA description of the templateOn the datasheet, this field appears as a text box labeled ML Description.

In this box, you can enter a description of the action users will be completing when they enter readings for this Checkpoint (e.g., Pump Check, Vibration Check, or Temperature Check).

This is a required field.

Include as Health Indicator SourceBooleanIndicates whether a potential health indicator source is used to create health indicators.In the datasheet, this field appears as a check box labeled Include as Health Indicator Source. When this check box is selected, health indicators are created for the selected source. When the check box is cleared, health indicators are not created for the selected source.
Maximum Target ValueNumericA number representing the highest target reading value that is acceptable for the Checkpoint

On the datasheet, this field appears as a text box labeled Maximum Target Value, in which you can enter a number. Together, the value stored in this field and the value stored in the Minimum Target Value field define a target range that appearson the More Information screen on a Windows Mobile device.

Note: This feature is not supported on tablet devices.

This field is disabled when the value in the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Target Value field with the value you enter in the Minimum Target Value field. If you enter a value in the Maximum Target Value field that is less than the value in the Minimum Target Value field, a message will appear, indicating that the value must be greater than the value in the Minimum Target Value.

Maximum Valid ValueNumericA number representing the highest reading value that is acceptable for the Checkpoint

On the datasheet, this field appears as a text box labeled Maximum Valid Value, in which you can enter a number. This value is used by the mobile device to check the reading value that is entered by the device user and display a message if the value they enter is higher than this value. Together, this value and the value in the Minimum Valid Value field define the valid value parameters for a reading.

Note: This feature is not supported on tablet devices.

This field is disabled when the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Valid Value field with the value you enter in the Minimum Valid Value field. If you enter a value in the Maximum Valid Value field that is less than the value in the Minimum Valid Value field, a message will appear, indicating that the value must be greater than the value in the Minimum Valid Value.

Minimum Target ValueNumericA number representing the lowest target reading value that is acceptable for the Checkpoint

On the datasheet, this field appears as a text box labeled Minimum Target Value, in which you can enter a number. Together, the value stored in this field and the value stored in the Maximum Target Value field define a target range that appears on the More Information screen on the mobile device.

Note: This feature is not supported on tablet devices.

This field is disabled when the value in the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Target Value field with the value you enter in the Minimum Target Value field. If you enter a value in the Minimum Target Value field that is greater than the value in the Maximum Target Value field, a message will appear, indicating that the value must be less than the value in the Maximum Target Value.

Minimum Valid ValueNumericA number representing the lowest reading value that is acceptable for the Checkpoint

On the datasheet, this field appears as a text box labeled Minimum Valid Value, in which you can enter a number. This value is used by the mobile device to check the reading value that is entered by the device user and display a message if the value they enter is lower than this value. Together, this value and the value in the Maximum Valid Value field define the valid reading value parameters for a Checkpoint.

Note: This feature is not supported on tablet devices.

This field is disabled when the ML Type field contains Character.

A rule exists on this field that will compare the value you enter in the Maximum Valid Value field with the value you enter in the Minimum Valid Value field. If you enter a value in the Minimum Valid Value field that is greater than the value in the Maximum Valid Value field, a message will appear, indicating that the value must be less than the value in the Maximum Valid Value.

ML TypeCharacterThe type of data that users can enter when creating a Reading linked to the Measurement Location

On the datasheet, this field appears as a list labeled ML Type and contains the following values:

  • Character. If you select Character, users can record any reading value for this Checkpoint.
  • Numeric. If you select Numeric, they must record a numeric reading value for this Checkpoint.
More InformationCharacterAdditional instructions about the Checkpoint that you want to be displayed on the Data Collection page

This field appears on the Data Collection page and is labeled Additional Instructions on that page.

Non-Compliance Date IntervalNumericIt is the Non Compliance Date Interval (in days) added to Next Date to get the Non-Compliance Date

This field is not populated automatically.

If Non Compliance Date Interval is absent, then Next Compliance Date value is populated as: Next Date + Schedule Interval.

ProductCharacterThe product produced by the piece of equipment that is associated with this Checkpoint

On the datasheet, this field appears as a cell. You can enter a value directly in the Product cell.

You can use this field to differentiate which Checkpoint is relevant depending on the current product for equipment that is used to produce multiple products. The field would be used as a filter in a customized download query to include only the relevant Checkpoints depending on the current product. This feature is only supported for Windows CE mobile devices that use a customizable download query.

Note: This feature is not supported on tablet devices.
Requires Equipment ShutdownBooleanIndicates whether the equipment requires shutdown

On the datasheet, this field appears as a check box, which is cleared by default.

ScheduleCharacterThe schedule by which you want to take readings for the Measurement Location TemplateThis field contains a ellipsis button that you can select to view the Schedule window, where you can define the schedule for the Measurement Location Template.
StatusCharacterThe status of the Measurement Location

On the datasheet, this field appears as a list labeled Status and contains the following values:

  • Active
  • Inactive

You can select a value from the list. This field contains the value Active by default.

Inactive Measurement Locations will not appear on Data Collection pages.

Template IDCharacterThe ID for the templateOn the datasheet, this field appears as a text box labeled Template ID. You can enter an ID for the template. This value must be unique. A rule exists on this field that will check whether the value that you enter in Template ID field is already used in a different Measurement Location Template. If the value is already used in a Measurement Location Template, a message will appear indicating that the ID already exists.
Unit of MeasureCharacterThe unit of measure that users can specify when entering a numeric reading value for the CheckpointOn the datasheet, this field appears as a list labeled Unit of Measure. You can select a value from the list. This field is disabled if the ML Type field contains the value Character.
Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Measurement Location contains all the values from the UOME system code table, sorted by their descriptions.

Operator Rounds Recommendation Records

Operator Rounds Recommendation records are created by mobile device users to communicate maintenance or follow-up inspection requirements based on the observed conditions of Checkpoints on a Route. Recommendations can be created linked to a specific Checkpoint and the related asset, or as standalone recommendations that are linked to the Equipment or Functional Location only.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

Note: When configuring offline forms, be careful to include only fields where field level rules are not used. In particular, fields that are required and disabled should be avoided. In many cases, field level rules may be replaced by field behaviors, which are supported in offline forms.

This topic provides an alphabetical list and description of the fields that exist for the Operator Rounds Recommendation family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive; instead, it is limited to field behavior that differs from General Recommendation fields.

FieldData TypeDescription
Assigned ToTextThe user to which the recommendation is assigned. This field appears in the Recommendations section of the RDC Overview page.
Created from Measurement LocationCharacterThe Measurement Location for which the recommendation was created
Created from Measurement Location AssetNumericThe asset that is associated with the Measurement Location for which the recommendation was created
Created OnDateThe date and time on which the recommendation was created. This field appears in the Recommendations section of the RDC Overview page.
DescriptionTextThe text that appeared in the Description cell when the Recommendation was saved on the mobile device
HeadlineTextThe text that appeared in the Headline cell when the Recommendation was saved on the mobile device
Measurement Location Entity KeyNumericThe Entity Key of the Measurement Location for which the recommendation was created
Recommendation IDNumeric

A value that identifies the recommendation record

Source ML DescriptionTextFor recommendations, other than standalone recommendations created on a mobile device, this field is populated automatically with the value that is stored in the ML or LR Description field in the Measurement Location or Lubrication Requirement record for which the recommendation was created.
TypeTextThe type of recommendation (for example, Operator Rounds Recommendation). This field appears in the Recommendations section of the RDC Overview page. This field is populated automatically.

Operator Rounds Recommendation In Error Records

Operator Rounds Recommendation in Error records are created when a recommendation saved on a device fails to upload to GE Digital APM for any reason. Operator Rounds Recommendation in Error records contain values from the data that was entered on the device.

The information in the topic reflects the baseline state and behavior of these fields. This list is not comprehensive; instead, it is limited to field behavior that differs from Operator Rounds Recommendation fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescription
Recommendation Error DetailsTextOn the Operator Rounds Recommendation in Error datasheet, this read-only field contains the details of the error that occurred when creating the recommendation fails.

Reading Records

Reading records store details about readings taken at Checkpoints on a Route. This topic provides an alphabetical list and description of the fields that exist for the Reading family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Action TakenCharacterThe action taken based on a readingYou can enter a value in this field.
Asset IDCharacterThe ID of the asset associated with the Checkpoint
When the reading is linked to:
  • Equipment, this field is populated automatically with the value in the Equipment ID field in the linked Equipment.
  • A Functional Location, this field is populated automatically with the value in the Functional Location field in the linked Functional Location.
CommentCharacterA comment about the readingThis field is populated with the text that a user entered in the Comments text box, which appears when taking a reading.
Reading Taken DateDateThe date the reading was takenThis field is populated automatically with the date on which you took the reading.
Reading Value CharacterCharacterThe character value of the readingYou can enter a value in this field.
Reading Value NumericNumericThe numeric value of the readingYou can enter a value in this field.
Related ML Entity KeyNumericThe entity key of the associated CheckpointThis field is populated automatically by the associated Checkpoint.
Related Route History Entity KeyNumericThe entity key of the associated route historyThis field is populated automatically by the current open route history record.
StatusCharacterThe status of the readingThis field is populated automatically with Complete, Ignored, or Non Compliant, based on the schedule of the Checkpoint.
Taken byCharacterThe user who recorded the readingThis field is populated with the user that took the reading.
Unit of MeasureCharacterThe unit of measure that users can specify when entering a numeric value for the readingThis field appears as a list populated by the UOME System Code Table.

This field is disabled if the value in the ML Type field is set to Character, or if the value in the LR Type field is set to Check Off.

Note:

Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

The UOM field for a Measurement Location contains all the values from the UOME system code table, sorted by their descriptions.

The UOM field for a Lubrication Requirement contains a subset of values from the UOME system code table based on specific reference values from the MI_LM_REFERENCES system code table.

Rounds Sequence Information Records

Rounds Sequence Information records store information about the order in which Checkpoints appear in a route.

Note: The values in Rounds Sequence Information records cannot be modified in Record Manager. These records are created or updated automatically to reflect the order in which Checkpoints are arranged within a route in Rounds Designer. Records are created or updated when you select Save Route Sequence, after the Rounds Designer page has been closed, or on a defined schedule.

This topic provides an alphabetical list and description of the fields that exist for the Rounds Sequence Information family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Checkpoint or Condition KeyNumericThe Entity Key of the Checkpoint or condition for which this record was createdThis field is populated automatically.
Rounds RankNumericThe location of the Checkpoint or condition within the Route hierarchyThis field is populated automatically and should not be modified.
Route KeyNumericThe Entity Key of the Route containing the CheckpointThis field is populated automatically.
SequenceNumericThe position the Checkpoint appears in a RouteThis field is populated automatically.

Route Records

This topic provides an alphabetical list and description of the fields that exist for the Route family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Last DateDateThe date on and time at which the Route status was changed to FinishedIf the Route has a Schedule, this field is populated automatically after the Route is marked done and uploaded to GE Digital APM.
Next DateDateThe date on and time at which the readings for the Route become dueIf the Route has a Schedule, this field is populated automatically based on the values in the Schedule field and the Last Date field. If the Last Date field is empty, the value in the Next Date field is calculated using the schedule and the current date and time.
Route DescriptionCharacterA description of the Route, which appears in the Description column in the Routes grid

On the datasheet, this field appears as a text box labeled Route Description, in which you can enter a description of the Route.

Route IDCharacterA name for the Route

The value in this field is used to identify the Route in the left pane, Route section, and on the mobile device.

Route Scan IDNumericThe scan ID that you want to assign to the RouteOn the datasheet, this field appears as a text box labeled Route Scan ID, in which you can type the scan ID.
SequenceTextThe sequence of Checkpoints and their successors on a RouteThis field is populated automatically and does not appear on the Route datasheet. It is disabled by default and should not be enabled or modified.
ScheduleCharacterThe schedule by which you want to take readings for the RouteThis field contains a ellipsis button that you can select to view the Schedule window, where you can define the schedule for the associated Route.
StatusCharacterThe status of the Route

On the datasheet, this field appears as a list labeled Status and contains the following values:

  • Active
  • Inactive

This field contains the value Inactive by default.

Routes will only be available in the Route Data Collection module if the Status is Active.

Route History Records

Route History records store information on all the Measurement Location readings taken, and also about the completion of a Route. This topic provides an alphabetical list and description of the fields that exist for the Route History family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

Note: Multiple In Progress Route History records may exist if multiple users have commenced taking readings on the same Route.
FieldData TypeDescriptionBehavior and Usage
Close DateDateThe date and time on which the Route status was changed to FinishedThis field is populated automatically after the Route is marked done.
Closed ByTextUser ID of person marking the Route done is saved to the fieldThis field is populated with the User id of the person marking the Route done. The field is formatted to show the user name.
CommentsTextComments about the RouteThis field is populated with the text that a user entered in the Comments text box, which appears when marking the Route as done.
Readings ExpectedNumberThe number of Checkpoints in the associated RouteThis field is populated automatically when the user has commenced taking readings on the Route. The value will continue to be updated automatically as readings are collected, until the Route is marked done. If the Route contains conditional Checkpoints, this field accounts only for the Checkpoints whose conditions were met.
Readings TakenNumberThe number of Checkpoints in the associated Route for which readings were takenThis field is populated automatically when the user has commenced taking readings on the Route. The value will continue to be updated automatically as readings are collected, until the Route is marked done.
Recommendations RaisedNumberThe number of recommendations created for routeThis field is populated automatically and displays the number of recommendations created for route. The value will continue to be updated automatically as recommendations are created, until the Route is marked done.
StatusCharacterThe status of the RouteThis field is populated with In Progress if a user has commenced taking readings, but has not yet marked the Route as done. After the Route has been marked done the field will be populated with Finished.