Workflow
Product Workflow
This workflow describes the process for comparing actual production to planned production to uncover any minor or major factors causing loss in production.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Define Codes
Persona: Solution Administrator
Define the event codes that are used to categorize the reasons for production losses and events.
Define Products
Persona: Solution Administrator
Define the type of commodities produced and offered for sale.
Define Production Unit
Persona: Solution Administrator
Define the type of production unit that represents the manufacturing processes.
Define Production Profile
Persona: Solution Administrator
Define what and how much each unit is capable of producing.
Create Plan Templates
Persona: Solution Administrator
Create Templated Plans for a Production Unit that may then be used to create actual production plans using a simplified wizard in the main application.
Create Production Plan (Manual/Time/Quantity/Template)
Persona: Analyst
Create a production plan by specifying the duration of the plan, how many products will be produced, how much of each product will be produced, and during which periods the products will or will not be produced.
Enter Production Data
Persona: Analyst
Enter the quantity of production for each of the products that was scheduled to be produced in a selected production period. Production Data entry can also be "automated" such that the production quantity is read into the Production Actual value from an OPC-compliant host system.
Reconcile Production Losses
Persona: Analyst
In cases where the Production Actual value is less than the Planned Production value an Unaccounted Loss will be created for the delta. Reconcile production losses to assign codes (e.g., OEE, Event, and Impact) and Production Events to account for the production losses.
Create Production Event
Persona: Analyst
Define a production event that causes shutdown, slowdown, or failure of production to meet the defined specification.
Assign Causing Asset
Persona: Analyst
Identify the cause of an event and assign that event to an asset.
Other Workflows
Persona: Analyst
Other workflows provide production data from: RCA, Bad Actors Charts, and Metrics and Scorecards.
Root Cause Analysis (RCA)
Persona: Analyst
See the RCA workflow.
Integrate with M2M Data Source
Persona: Solution Administrator
OPC Integration can be used to provide actual production data.
Go to the Integrate with M2M Data Source workflow.
Policy Designer: Design Policy
Persona: Analyst
Create Production Events and send email notification using Policy Designer. Once the event has been created, the PLA user will be able to enter the remaining details addressing why the event occurred.
Go to the Policy Designer: Design Policy workflow.