Working with Protocol Adapters
About the Protocol Adapters
The APM OT Connect Adapter Service can support several different Protocol Adapter modules, depending on the configuration of the corresponding OT Source. These Protocol Adapters are used to connect to a specific Process Historian or a server that complies with an OPC specification.
- Service Start
- When the OT Source is reconfigured
Capabilities
Different Protocol Adapters, and even in some cases different implementations or versions of a Process Historian or OPC Server can support a variety of different capabilities when querying or subscribing to data.
The supported capabilities are listed on the table below:
Name | Supported action |
---|---|
LastReading | Query the OT Source for the last good Reading for a Tag. |
StartToEndReadings | Query the OT Source for all Readings between a Start and End time. |
SubscribeReadings | Establish a subscription to new Readings for a Tag, which can be used to update Health Indicators or trigger Policy Instances unsolicited. |
BeforeEndReadings | Query the OT Source for a specified number of readings before an End time. |
SubscribeReadings | Subscribe to a Tag for updated Readings with a new Timestamp or Value. |
The Capabilities of an OT Source are reported as part of the Connection Status.
Simulation
The Simulation Protocol Adapter is provided for testing and exploration. Rather than connecting to an actual process historian, it provides simulated tag metadata and Readings for all Capabilities.
ProtocolConnection
The Simulation Protocol Adapter is not configurable.
OPC-HDA
The OPC-HDA Protocol Adapter can connect to an OPC Classic HDA 1.20 server.
Vendors have implemented different elements of the specification, so it is important to review the Connection Status or OT Source Capability Utility report to understand what Capabilities are available from the server you want to integrate with APM.
- LastReading
- SubscribeReadings
- GetStartEndReadings
ProtocolConnection
The OPC-HDA ProtocolAdapter requires the ProgId to be configured.
If the correct ProgId is not provided, the ProtocolAdapter will log an exception report on all available OPC-HDA ProgIds on the server on startup.
Optionally, the BatchSize can be configured to support OPC-HDA servers with an unusually low or high limit to the number of records that can be returned for a single request.
OSI PI
The OSI PI protocol adapter can connect to PI Server 2010 and later, using the Asset Framework (AF) protocol. This allows OT Connect to support PI without an intervening OPC server. OSI PI protocol adapter requires the PI AF Client to be installed on the OT Connect Process Data server. The AF protocol offers improved security, performance, and reliability. Therefore, it is recommended to use this adapter to connect to the OSI PI servers.
- LastReading
- SubscribeReadings
- GetStartEndReadings
- GetBeforeEndReadings
Configure the OSI PI Protocol Adapter
- Install PI AF Client. For information on installing the PI AF client, refer to the OSIsoft documentation.
- Configure the OT Source.
Host Name | Hostname or the FQDN of the target server. The host name must exactly match with the name that is configured in the System Explorer. |
User Name | Windows user configured with a PI mapping. |
Password | Windows password. |
Proficy Historian
The Proficy Historian Protocol Adapter can connect to Proficy Historian 4.0 and later through the Client Access API. This allows OT Connect to support the Proficy Historian without an intervening OPC server. It requires the Client Access Assemblies to be installed on the OT Connect Process Data server.
It is recommended to use this adapter to connect to the Proficy Historian servers whenever possible, as the Client Access API offers improved security, performance, and reliability.
- LastReading
- SubscribeReadings
- GetStartEndReadings
- GetBeforeEndReadings
Configure the Proficy Historian Protocol Adapter
- Install the Historian Client Tools by selecting the Client Access Assemblies. For information on installing the Historian Client Tools, refer to the Proficy Historian documentation. Other features are not required and the Historian Data Archiver can be on another server.
- Configure the OT Source.
Host Name | Hostname or FQDN of the target server. The host name must match exactly with the name that was provided when installing the target historian. |
User Name | Windows user with iH Readers membership on the Process Historian server. |
Password | Windows password. |
OPC-DA
The OPC-DA Protocol Adapter can connect to OPC Classic DA 3.0 servers
While some OPC-DA 2.0 – 2.05a servers are forward compatible, and the OT Connect OPC-DA ProtocolAdapter can work with them, this varies between vendors, and is not guaranteed.
Only OPC 3.0 servers are officially supported by OT Connect.
The OSI Pi OPC-DA Server is an example of a 2.05a server that is not compatible with OT Connect.
Vendors have implemented different elements of the specification. So, it is important to review the Connection Status or OT Source Capability Utility report to understand what Capabilities are available from the server that you want to integrate with APM.
For OPC-DA, the most common limitation is properties, such as Description or RawUom not being available for Tag Sync, which will complete with only the Tag Name and DataType.
- LastReading
- SubscribeReadings
ProtocolConnection
The OPC-DA ProtocolAdapter requires the ProgId to be configured.
If the correct ProgId is not provided, the ProtocolAdapter will log an exception report on all available OPC-DA ProgIds on the server on startup.