Workflow

OT Connect Workflow



A1 - Define connection to OT Source

Persona: Solution Administrator

Define OT Source connection endpoint. Standard OT Source interfaces offer connection to field device systems, such as condition monitoring devices, instrumentation, process historians, and so on.

A2 - Define Data Acquisition Parameters of OT Source

Persona: Solution Administrator

Define parameters for the acquisition of data from the OT Source in APM. These parameters can include data polling frequency (that is, how often data will be acquired and aggregated for evaluation), filtering (for example, severity and type of data), and so on.

A3 - Test connection to OT Source

Persona: Solution Administrator

After the data acquisition parameters are defined, test the connection to ensure that the OT Source is communicating with APM.

A4 - Synchronize Source Tag Metadata from OT Source

Persona: Solution Administrator

An initial data synchronization is conducted that creates records representing Tags in APM. A Source Tag can represent a time series of data for a single monitored parameter, a summarized or calculated result, or a stream of events. Tags are kept in synchronization with changes in the field data systems. If a Tag used in APM is removed from the source system, the deleted Tag will be flagged as deleted. The Tag will not display in the user interface, but will remain in the APM database.

A5 - Preview Source Tag Data

Persona: Solution Administrator

Interrogate synchronized Tags from APM to confirm data delivery and coherence.