Specifying the Warning Period
About this task
The warning period represents the number of minutes before a session limit or idle limit is reached when users are warned they are about to be disconnected or logged off. For example, if the warning period is set to 2, users will be warned 2 minutes before the session limit or the idle limit is reached.
The warning period must be less than the session limit and idle limit settings. This feature is disabled by default.
Procedure
- From the Webspace Administration, in the server tree, select the desired server from the list.
- On the Tools menu, click Host Options. The Host Options dialog box appears.
- Click the Session Shutdown tab.
-
Select the Warning
period check box.
Note:Either a Session or Idle time-out must be configured for the Warning period check box to become available.
- In the field next to the check box, enter the number of minutes before a session or idle limit is reached when users are warned that they are about to be disconnected or logged off.
- Click OK.