Specifying the Session Limit
About this task
The session limit is the number of minutes that sessions are allowed to run on a Webspace Server.
Procedure
- From the Webspace Admin Console, in the server tree, select the desired server from the list.
- On the Tools menu, click Host Options. The Host Options dialog box appears.
- Click the Session Shutdown tab.
- Select the Session check box.
- In the field next to the check box, enter the number of minutes that a session is allowed to run on a server before its user is logged off.
-
Click OK.
The minimum number of session time is 1 minute, and the maximum is 44640 minutes (31 days). This feature is disabled by default.