Command-Line Options

Use the Project Deployment Tool command-line options to bundle and deploy a Web HMI project to another node.

The following Project Deployment Tool command-line options are case-sensitive.
OptionDescription
--bundleCreates a bundle containing project data.
--deployDeploys a bundle in the target, overriding the current project data.
--scadaBundles or deploys the HMI/SCADA contents. Used in conjunction with the bundle and deploy options.
--webserverBundles or deploys the Web HMI contents. Used in conjunction with the bundle and deploy options.
--serverSpecifies the web server instance URL in which to create or deploy a bundle.
--usernameSpecifies your Web HMI user name for authentication.
--passwordSpecifies your Web HMI password for authentication.
--fileSpecifies a file name for your bundled content.

If you do not specify a file name, the tool generates a name that includes the server name and time stamp.

--overwriteWithout prompting, automatically overwrites the target files with your source files.
--iFixAllows you to pass in non-default parameters to the iFIX backup and restore tool, which bundles and deploys iFIX content. The supplied parameters overwrite the default parameters.

The default parameters are:

  • Bundling  �� "/S /BackupSec", which performs a full backup with security files in silent mode.
  • Deployment:  �� "/S /RestoreSec", which restores <xxxxx>, replacing the current security settings with those in the bundle file.

To pass in more than one parameter, surround the parameter value in double quotes, such as: --iFix="/F /S"

Unsupported parameters (/B, /R, /FactoryDefaults):

  • /B and /R  �� The Project Deployment Tool determines the right operation based on the --bundle or --deploy options.
  • /FactoryDefault parameter  �� You cannot use the Project Deployment Tool to bundle or deploy iFIX factory defaults.

For more information on the iFIX backup and restore tool, see the iFIX online documentation.

--helpDisplays the supported command-line options.