Scopes for iFIX Users/Groups
This topic provides a list of scopes you can assign to users/groups for accessing iFIX.
Refer to the following table to assign access to specific areas/functionalities of iFIX:
Scope | Description |
---|---|
scada.fix_shared_IFIX_PROFICY_AUTH_ADMIN |
Allows access to all iFIX application features. Any Proficy
Authentication user who is a member of this group will have privileges similar
to a native iFIX ADMIN user (except the access to security areas). Proficy
Authentication users who want to directly log in to iFIX can use this
group. This group is not available by default when you upgrade from iFIX 6.1 or 6.5. You must manually create this group with all the iFIX application features as needed. |
scada.fix.shared.APPLICATION_DESIGNER |
Allows a user to access Configuration Hub and provides use of iFIX
features such as iFIX connection, database, and model management. Important: scada.fix.shared.APPLICATION_DESIGNER is not available
by default when you upgrade from iFIX 6.1 or 6.5. You must manually create
the group with the required iFIX application features, or update your
existing groups to include the following iFIX application features (if you
want users in these groups to have access to and use Configuration Hub).
|
scada.fix.shared.OPERATORS |
Allows run mode only access for a user in iFIX. |
scada.fix.shared.SUPERVISORS |
Allows access to WorkSpace run and configure mode, as well as access to background task exit, iFIX system shut down, and iFIX system user login. |
scada.proficy.admin: |
Allows the Proficy Authentication user access to the iFIX Projects panel and to the Deploy operations from Configuration Hub. This group is for Proficy Authentication only; this group is not linked to any iFIX group and has no permissions in iFIX. |