About this task
You can skip an operation that is configured as optional.
Before you begin
- If you do not have the permission to perform this task, a message appears, stating the same. In such case, request your administrator to provide the permission using Security.
- You can only skip an operation that is configured as Optional. You can specify an operation as optional using Route Editor.
- Ensure that the optional operation is in Ready status.
Procedure
-
In the Work Queue page, in the row containing the optional operation that you want to skip, select the SKIP button under COMP/REC column.
Alternatively, you can select the operation and work order combination from the
Work Queue page, and then select the
SKIP button in the page heading.
Note: You can identify an operation as optional using the
OPT column. You can add the
OPT column using

.
The Select Serial number(s) to Skip window appears displaying all the serials/lots of the operation that are in Ready status.
-
If you want to skip all the available serials/lots, select the check box in the heading row of the table. If you want to skip specific serials/lots, perform one of the following steps:
- Select the check box for each serial/lot that you want to skip.
- Search for a serial/lot by entering the value in the Search in available serial numbers box, and then select the check boxes from the filtered list that appears.
- Scan the bar code of the serial/lot by selecting
.
-
Select the Skip button to skip the operation.
The selected serials/lots are skipped.