Add Applied Time for a Work Order

About this task

To add the applied time for a work order, you must create a labor record.
Note: Once a labor record is created and submitted, an operator or a supervisor cannot delete it.

Procedure

  1. In the Time Booking page, in the View By box, select a time period to view the labor records.
  2. Select Add New Record and select the type of labor record you want to add.
    A blank row with the selected labor type is displayed.
  3. Provide values as specified in the following table:
    ColumnDescription
    Work OrderEnter the work order name of the selected labor type for which you want to add the applied labor time.
    Serial/Lot#Enter the serial or lot number associated with the work order.
    OperationEnter the type of operation for which you want to add the applied labor time.
    MachineEnter the name of the machine for which you want to add the applied labor time.
    Applied TimeEnter the time range, in HH:MM format, that you want to add as applied time for this labor record.

    Alternatively, you can also select the <insert clock icon> and select the time range from the list

    Note:
    • If you have selected a labor of type Direct, the information that is populated in the Work Order, Serial/Lot, Operation, and Machine columns are of the same type.
    • Only work orders that are ready, in-progress, and completed are populated in the respective fields.
    • If you add an indirect labor record, then the fields Work Order, Serial/Lot, Operation, and Machine are not mandatory. However, you must select the reason from the Select reason for Indirect Labor window. The reasons that are displayed in the Select reason for Indirect Labor window are based on the configuration made under the Sample_Labor_Indirect reason tree in the Plant Applications Administrator.
  4. To create more labor records, repeat steps 2 through 4.
    Tip:
    • To cancel the current record, select X.
    • To cancel all the records that you are currently creating, select Cancel.
  5. Select Submit.

Results

The labor records are added to the table.