Server name | Enter the server name where the Plant Applications database is installed in the format HOST_NAME\INSTANCE . Where HOST_NAME is the host name (either a fully qualified domain name or IP address, of the server) and INSTANCE is the instance of the server used by the database.Note: If there is no instance for the server, you can enter HOSTNAME as the server name. Localhost is not an acceptable value for HOSTNAME . |
Database | Enter the name of the Plant Applications database for which you want to apply the schema changes to accept the Unicode characters. |
User name | Enter the user name that has permissions to access the database you entered in the Database box. By default, the user name appears as sa . |
Password | Enter the password for the user name you entered in the User name box. |
Port | Optional: Enter the number of the port that the instance uses to listen for client connections. Note: The default port is 1433. |