Plant Applications Client

The Plant Applications Client provides a customizable environment for using Plant Applications Views and Displays to access your plant data. For more information about using the Plant Applications Client, refer to Plant Applications Help.

Legend:

  1. A View is a group of displays that can be opened at the same time. Views are created in the Plant Applications Client.
  2. The toolbar provides a quick way to perform tasks specific to the active display. The toolbar automatically changes depending on which display is active.
  3. The box indicates the status of the connection to the Plant Applications Server. Green indicates the connection is active.
  4. This area displays the name of the person who is currently logged in to the Plant Applications Client.
  5. Click the tabs to switch between displays.