View the Details of an Event
- Event Information
- Waste Cause Information
- Waste Variables
Event Information
Field | Description |
---|---|
Event | The production event to which the waste is associated. By default, 500 records will be displayed. As you scroll down and reach the end of the list, you can select More to display 500 more records. Note: This field is populated only for a production-based event. In case of a time-based event, this field is blank. |
Created On | The date and time the waste event record was created. |
Updated On | The date and time the waste event record was updated. |
Amount | The amount of waste that was generated for the event. |
Units | The unit of measurement that correspond with the amount of generated waste. |
Product | The product that was being produced. |
Added By | The name of the service or person who created the waste event. |
Waste Cause Information
Field | Description |
---|---|
Location | The specific piece of equipment along a production line that caused the waste. |
Fault | The error in the processing stream or equipment that led to generation of waste. |
Type | The physical state of waste that was generated. |
Waste Reason | The reason that describes the cause of the waste. |
Waste Action | The corrective action taken to fix the fault that caused the waste. |
Waste Variables
This section splits the production event into different timelines according to the amount of waste that was generated every time the production event was triggered. The final entry displays the overall waste that was generated for the entire production event.