The ERP Export service publishes messages in a JSON and/or B2MML format to the following tables:
Events |
Table |
- mes.erp.outbound.messages.ClockOffEvent
- mes.erp.outbound.messages.ClockOnEvent
|
erp.erp_integration_outbound_laborVouchering_messages |
- mes.erp.outbound.messages.MaterialLotStatusChangedEvent (event generated when a serial/lot is scrapped, a receiver is completed, or a non-conformance is raised for a material/lot in a receiver)
- mes.erp.outbound.messages.OperationCompletedEvent
- mes.route.releasedRoutes.RouteReleasedEvent
|
erp.erp_outbound_integration_standard_messages |
The table contains the following columns:
Column | Description |
---|
Id | The ID of the message. |
Event_Type | The type of the event. |
Message | The body of the message. |
Inserted_By | The user or the system that sent the message. |
Inserted_Date | The date on which the message was initiated. |
Message_Type | The format of the message (application/xml or application/JSON). |