Configure ERP Integration
The following table provides the sequence of steps that you must perform to configure ERP integration. You must provide your UAA credentials to perform these steps.
Step Number | Description | Notes |
---|---|---|
1 | Provide mapping details of a work order, process order, or material. | This step is required if the work order, process order, or material details are stored in a B2MML or XML file. It is used by the ERP Transformation service to convert the file to a JSON file. |
2 | Connect to the ERP Integration database by configuring the database settings, and insert records. | This step is required. After the integration, work orders, process orders, and materials are automatically imported to the ERP Integration database. |
3 | Configure the ERP Scheduler service parameters. | This step is optional. It is used to change the default value of the time interval at which the ERP Scheduler service polls the ERP Integration database. |
4 | Configure the ERP Import service parameters. | This step is optional. It is used to change the default values of parameters used in the service (such as names of property categories and groups). |
5 | Configure the ERP Export service parameters. | This step is optional. It is used o change the default values of parameters used in the service. |