Configuration Parameters in the ERP Import Service
Parameter | Description |
---|---|
Workorder_post_delete_delay | The duration after which importing a work order of the same name replaces the existing work order. The default value is 15 seconds. Note: This parameter is only applicable for importing work orders. |
Workorder.property.group.id | The GUID of property group with the name WorkOrder Import from Property Definition application. This group Id belongs to WorkOrder Import. The default value is CB21B6A6-B370-46D5-8400-5BA64C46CB9F. |
Material.property.group.id | The GUID of property group with the name Material Import from Property Definition application. This group Id belongs to Material Import. The default value is 79433EC1-6683-4BED-B353-BD667210E0A2. |
maximumCacheSize | The maximum number of entries that the cache can contain. The default value is 100. |
cacheExpireAfterWrite |
Specifies that each entry be removed from the cache after a fixed duration after one of the following events occur:
The default value is 5 minutes. |
- The parameters Workorder_property_Group_name and Material_property_Group_name in Plant Applications Web Client version 8.0 are changed to Workorder.property.group.id and Material.property.group.id.
- The parameters Workorder_property_category_name and Material_property_category_name are not used in Plant Applications Web Client version 8.1.
Configuring parameters in the Property Definition application
In Plant Applications Web Client, access the Property Definition page, select Erp App in the CATEGORY box, and then select MaterialLot Import in the GROUP box.
Parameter | Description |
---|---|
inventory.line.id | The GUID of property definition with the name Inventory Line from Property Definition. The default value is AF651BC5-4161-4B03-8124-DE2AE4887CCE. |
OrgCode | The GUID of organization code of the material lot from Property Definition. This property is used to import receivers with material lots from the ERP application. For each material lot, the combination of the organization code and the units of measure must be unique. |
receiver.line.id | The GUID of property definition with the name Receiver Line from Property Definition. The default value is 02651301-05BD-4DE0-999C-0B6F93630308. |
receiver.status.id | The GUID of property definition with the name Receiver Status from Property Definition. The default value is FFDEE988-8E13-43C4-8BC3-A379BC6ACA53. |
receiver.unit.id | The GUID of property definition with the name Receiver Unit from Property Definition. The default value is 0716041E-DFC6-4939-A81C-B2EB8F25B29E. |
Add default groups and definitions
If you delete the default groups and/or definitions from the database, get the GUIDs of created groups and/or definitions from the database and modify the GUIDs with the new values in application.properties file (for non-docker environment) and/or environment variables (for docker environment) of the ERP Import service.