Configuring Parameters for the ERP Import Service
This topic describes the various configuration parameters that a system administrator must configure in ERP Import service and the Property Definition application in Plant Applications Web Client.
Note: The maximum number of properties that you can create per property group is 2000.
As a system administrator, you must configure the following values during installation. To change the configuration, restart the application.
Parameter | Description |
---|---|
material.property.group.id | The GUID of property group with the name Material Import from Property Definition application. This group Id belongs to Material Import. The default value is 79433EC1-6683-4BED-B353-BD667210E0A2. |
OrgCode | The GUID of organization code of the material lot from Property Definition. This property is used to import receivers with material lots from the ERP application. For each material lot, the combination of the organization code and the units of measure must be unique. |
workorder.property.group.id | The GUID of property group with the name WorkOrder Import from Property Definition application. This group Id belongs to WorkOrder Import. The default value is CB21B6A6-B370-46D5-8400-5BA64C46CB9F. |
materiallot.property.group.id | The GUID of property group with the name MaterialLot Import from Property Definition application. This group Id belongs to MaterialLot Import. The default value is 170d56ca-1f50-47db-8e2b-793a792ad6c9. |
inventory.line.id | The GUID of property group with the name Inventory Line from Property Definition application. The default value is AF651BC5-4161-4B03-8124-DE2AE4887CCE. |
receiver.line.id | The GUID of property definition with the name Receiver Line from Property Definition application. The default value is 02651301-05BD-4DE0-999C-0B6F93630308. |
receiver.status.id | The GUID of property definition with the name Receiver Status from Property Definition application. The default value is FFDEE988-8E13-43C4-8BC3-A379BC6ACA53. |
receiver.unit.id | The GUID of property definition with the name Receiver Unit from Property Definition application. The default value is 0716041E-DFC6-4939-A81C-B2EB8F25B29E. |