Work Order Schema

Work orders are created for a specific product and must be completed on a production line. You can create work orders manually using Work Order Manager, and Route Editor applications. The work order schema information can be used to generate reports that are helpful in identifying and resolving the issues in plant operations.

Table 1. Work Order
Column Name Description
CreatedOn Work order created date and time.
CreatedBy The user who created the work order.
LastModifiedOn The latest date and time at which the work order was modified.
LastModifiedBy The user who modified the work order.
ConcurrencyToken System Fields.
Id Work Order identifier (Id).
Name Unique name for the work order.
RouteDefinitionId Route associated with the work order or Route Id.

(route.Route)

SegmentsDefinitionId Id of the Segment Definition Document.

(Segments Definitions table)

PP_Id Event dimension and variable values when PE was bound to Process Order (PP_Id).
PL_Id Planned Line on which the work order will be executed or Planned Line Id.
Prod_Id Production Line on which the work order is executed or Production Line Id.
Status Status of the Work Order:

10 - Not Ready

20 - Ready

30 - In Progress

40 - Complete

50 - Cancelled

PlannedStartDate The planned date and time to begin work on the work order.
PlannedEndDate The planned date and time to complete the work on the work order.
PlannedQuantity Quantity of product planned to manufacture as part of the work order.
DiscreteVirtualUnitId Production Unit Id, where the lots are created.
NumberOfIncompleteMaterialLotActuals Number of incomplete Material Lot Actuals.
Priority Priority in which the work order must be completed.
CancelledOn The date and time at which the work order was cancelled.
CompletedOn The date and time at which the work order was completed.
ReadyOn The date and time at which the work order is ready to be processed.
StartedOn The actual start date and time of the work order.
CompletedBy The user who completed the work order.
Table 2. Material Lot Actuals
Column Name Description
Id Id of the Material Lot Actuals.
LotIdentifier Lot name/Serial Number.
WorkOrderId Work Order Id.
Status Status of the Material Lot Actuals:

21 - Not Started

30 - In Progress

40 - Complete

ConcurrencyToken System Fields.
NumberOfIncompleteSegmentActuals Number of incomplete operations.
NumberOfActiveLotHolds Number of Holds.
PlannedQuantity Planned Quantity.
InitialPlannedQuantity Initial Planned Quantity.
ProductionEventId Production Event for the lot (Events Table).
CreatedBy The user who created the Material Lot Actuals.
CreatedOn The date on which the user created the Material Lot Actuals.
CancelledBy The user who cancelled the Material Lot Actuals.
CancelledOn The latest date and time at which the Material Lot Actuals was cancelled.
Table 3. Segment Actuals
Column Name Description
Id Id of Segment Actuals.
MaterialLotActualId Id of Material Lot Actuals.
SegmentId Operation's Segment Id inside Segments Definition Document.
PU_Id Production Unit Id, where the operation is executed.
Status Status of the Segment Actuals:

10 - Not Ready

20 - Ready

30 - In Progress

40 - Complete

50 - Cancelled

60 - Skipped

70 - Excluded

NumberOfActiveOperationHolds Number of Active Operation Holds.
CompletedBy The user who completed the work order.
CompletedOn The date and time at which the operation was completed.
ReadyOn The date and time at which the operation is ready to be started.
StartedBy The user who clocked-on the operation.
StartedOn The actual start date and time of the operation.
CompletedQuantity Quantity completed.
ProductionEventId Production Event Id (Events table) for the operation.
UserDefinedEventId User Defined Event Id for the operation.

(User Defined Events table)

Table 4. Complete Quantity Records
Column Name Description
Id Id of Complete Quantity Records.
SegmentActualId Operation's Segment Actual Id.
QuantityCompletedBy The user who performed the operation on the quantity.
Quantity The quantity of the lot on which you have performed the operation.
QuantityCompletedTime The date and time at which an operation was completed on the quantity.