Troubleshoot Time Series Data
Configuration Fields
Errors may occur when the following configuration fields contain incorrect values:
asyncFetchMode
Asynchronous queries are not supported in all Time Series Data environments. The following matrices show the results of Async and Dynamic queries based on the value of asyncFetchMode and whether the environment supports asynchronous queries.
asyncFetchMode | Async Query Result | Dynamic Query Result |
---|---|---|
true | Query returns a correlation ID. | Query returns either a correlation ID or data, depending on the date range of the query. |
false (default) | Query returns HTTP status code 400 Bad Request. | Query is translated to the Sync fetch type and returns results synchronously. |
asyncFetchMode | Async Query Result | Dynamic Query Result |
---|---|---|
true | Query returns HTTP status code 400 Bad Request. | Query returns HTTP status code 400 Bad Request. |
false (default) | Query returns HTTP status code 400 Bad Request. | Query is translated to the Sync fetch type and returns results synchronously. |
Time Series Data Delete Service
The Time Series Data Delete service may produce errors in response to service requests.
v2/time_series/delete
The following table contains errors that may occur as a result of requests made to the v2/time_series/delete
endpoint.
HTTP Status Code | Message | Cause |
---|---|---|
403 | Access Denied | The user does not have access permission to the Delete Timeseries scope. |
400 | You either do not have sufficient privileges for the requested tags or the tags were not found. | The user does not have access permission to the asset to which the tags apply. |
400 | Start time is missing. Please provide a start time. | A start time was not provided. |
400 | End time is missing. Please provide an end time. | An end time was not provided. |
400 | The tag list is empty. Please provide a tag in the tag list. | No tags were provided in the tag list. |
400 | Invalid Start Time. Start time cannot be less than -773094113280. | The start time was before Tuesday, July 3, 1945 3:38:06.720 AM GMT. |
400 | Invalid End Time. End time cannot be greater than 7730941129200. | The end time was after Monday, December 26, 2214 11:38:49.200 AM GMT. |
None | Delete time range does not span exact hours. | On shared clusters, the start time must be the beginning of an hour (for example, nn:00:00.000), and the end time must be the end of an hour (for example, nn:59:59.999). |