Time Series Data Sources
About Time Series Data Sources
The Time Series Data Source Configuration provides methods to configure connections to the time series data sources, and to manage and retrieve connection information. Currently, for Predix and SmartSignal data source types, this service supports connections to Predix Essentials instances of Predix and SmartSignal (instances that are deployed along with Predix Essentials). This service supports Proficy Historian and External Predix Data as its external data source connection.
To ensure that connectivity and resources can be accessed as needed, make sure the following JSON fields are configured correctly:
JSON Field | Description |
---|---|
alias | A unique alias name to save the data source configuration for the tenant. The alias name field in the application and JSON field must match. |
precisionLevel | The default precision level for the time-series data points. If no precision level is indicated during retrieval, the default value is used. |
authHost | The authorization host URL of the data source, for example, https://fssfed.stage.ge.com. |
auth | The authorization token URI to retrieve the authorization token to connect to the data source host, for example, /fss/as/token.oauth2.
|
authRequired | The boolean value to indicate if authorization is required to connect to the data source host. |
clientId | The OAuth client ID required to access the OAuth client. |
clientPwd | The OAuth password required to access the OAuth client. |
grantType | The authorization grant type. The default value is client_credentials. |
authHeaderParams | Header parameters required to retrieve the authorization token. |
authQueryParams | Query parameters required to retrieve the authorization token, for example, scope:api.
|
serviceHost | The service URL to retrieve time series data. |
interpolated | The URI to retrieve interpolated data, for example, /osmdatalayer/data/interpolated . |
raw | The URI to retrieve raw data, for example, /osmdatalayer/data/interpolated. |
current | The URI to retrieve sample data, for example, /osmdatalayer/data/sampled.
|
write | The URI to write back time series data into the Proficy data source. |
serviceHeaderParams | Header parameters required to pass to the service URL to retrieve the time series data. Note: Only define the service headers in the configuration if it is applicable to all types of time series data retrieval such as raw, current, and interpolated.
|
serviceQueryParams | Query parameters required to pass to the service URL to retrieve the time series data. Note: Only define the query parameters in the configuration if it is applicable to all types of time series data retrieval such as raw, current, and interpolated. If not properly defined, data retrieval may fail.
|
asyncFetchMode | Indicates whether the data source supports asynchronous queries. The default value that appears is false. Any value other than true is false. If your data source supports asynchronous queries, change the value to true. Attention: If you are unsure about the configuration, do not change the value. |
JSON Field | Description |
---|---|
alias | A unique alias name to save the data source configuration for the tenant. The alias name field in the application and JSON field must match. |
precisionLevel | The default precision level for the time-series data points. If no precision level is indicated during retrieval, the default value is used. |
ingestURI | The ingestion endpoint of the data source. |
ingestUserName | The user name to connect to the ingestion endpoint. This is not the Time Series Data ingestion credential. The value of ingestUserName is specific to the External Predix Time Series data source being configured. |
ingestPassword | The password to connect to the ingestion endpoint. This is not the Time Series Data ingestion credential. The value of ingestPassword is specific to the External Predix Time Series data source being configured. |
interpolationMode | The modes for interpolating data. These modes are initiated by entering either of these case-sensitive values: Math or Historian. In Math mode, Time Series Data returns empty data when interpolating a time period. Time Series Data returns zeros for Historian. You do not have to enter a value for this field if you prefer Math mode. |
authUrl | The URL to access the resource. |
authClientId | The OAuth client ID required to access the OAuth client. |
authClientSecret | The OAuth password required to access the OAuth client. |
authHeader | The authorization header type. The default value is Bearer. |
authType | The authorization type. The default value is ZAC. |
predixTsZoneID | The Predix Time Series service zone ID. |
zoneTokenScopes | The Predix Time Series service zone token scope. Scopes are permissions associated with an OAuth Client to determine user access to the resource through the application. |
queryURI | The query URI for retrieving time series data. |
extension | (Optional) This numeric value is represented in milliseconds. When configured, the interpolation query uses this time to control the start and end of the query bound intervals. If not configured or the value is configured as 0, then this parameter is ignored and the interpolation will look to fetch the start and end time data from infinite time. Note: This feature is currently not available in any Predix Essentials tenants in the US East. |
asyncFetchMode | Indicates whether the data source supports asynchronous queries. The default value that appears is false. Any value other than true is false. If your data source supports asynchronous queries, change the value to true. Attention: If you are unsure about the configuration, do not change the value. |
Assign a Default Time Series Data Source
Before You Begin
Procedure
- In the module navigation menu, select .
- In the Time Series Data Sources section, select the radio button next to the name in the Default column.
- The changes will be saved automatically.
Modify an Existing Time Series Data Source
Use the Time Series Data Source page to modify an existing time series data source.
Before You Begin
Procedure
- In the module navigation menu, select .
- In the Time Series Data Sources section, select
next to the name you want to modify.
- Modify the JSON file. Make sure you have provided all the required key value pairs for a successful configuration of the data source you are modifying.
- Select Save to permanently save your changes. Or, select Cancel to return to the Time Series Data Sources page without any changes.
Modify an Existing Time Series Data Source with Incorrect Value
Use the Time Series Data Source page to modify an existing time series data source with incorrect value.
Before You Begin
Procedure
Delete a Time Series Data Source
Before You Begin
You cannot delete SmartSignal or Predix Time Series data source types.