Dashboard Views
About Dashboard Views
Dashboard views allow you to add and display cards in the card library, which in turn allow you to add, display, and configure widgets associated with an asset context.
Dashboards are categorized by asset instance or class. Asset instances are associated with a class, where class is a generalized category of assets and instance is a specific asset. For example, an asset instance might be a specific GE turbine, whereas the associated class might be all GE turbines. You can designate a dashboard view as an instance, a class, or none. When you designate a dashboard view as a class, selecting an asset context (asset instance) that is part of the class displays the dashboard.
You can add a new dashboard using the Dashboard browser by selecting Create New. Once created, you change the name of the dashboard view, designate the dashboard view as an instance, a class, or none, designate the dashboard view as a public or private dashboard, set the permissions for the dashboard or display the dashboard summary card for the dashboard view, and save the dashboard. You can also enable asset filtering for the dashboards, or time filtering at the dashboard level.

- Add new cards to a dashboard view.
- Refresh or pause data for the widgets on the selected view.
- Set the current view as the default dashboard for the asset instance or classification.
- Export dashboard images with data as a PDF.
- Set the current dashboard as a favorite, allowing you to access the dashboard in My Favorites menu on the navigation bar.
- Does not apply to Predix Essentials: Make the current dashboard the home dashboard.
- View all your dashboards under the All Dashboards menu.
- Configure the Dashboard Summary card.
- Filter by time span.
- Filter by asset.
- Modify an existing dashboard view.
- Delete an existing dashboard view. Note: Deleting a dashboard deletes all the associated cards and widgets and cannot be undone.
- Return to dashboard browser.
Access the Dashboard Browser
Accessing the Dashboard Browser is the first step in managing your dashboards.
Procedure
Add the First Dashboard to an Asset Context
If no dashboard has been configured for an asset selected through the Context Browser, you can add a dashboard to the selected asset.
Procedure
Create, Modify, and Delete Dashboards
Once created, you can modify or delete dashboards that are associated with an asset instance, asset classification, or no classification.
About This Task
You can customize your asset view by creating a new dashboard in the Dashboards module.
Procedure
Designate the Dashboard Availability
About This Task
Procedure
- To designate dashboard availability to the asset instances associated with an asset class:
- To set the visibility of the dashboard:
Assign and Remove a Default Dashboard for an Asset
When you select an asset instance or asset class in the Context Browser, the default dashboard for that asset type appears. You can assign a configured view as default for the selected asset type.
About This Task
Dashboards | Sequence |
---|---|
Default asset instance | Default asset instance is displayed first, followed by additional views in chronological order. |
Default asset instance and default asset class | Default asset instance is displayed first, followed by default asset class, then additional views in chronological order. |
Default asset class | Default asset class is displayed first, followed by additional views in chronological order. |
No default dashboards | Views are displayed in chronological order. |
Procedure
Set a Favorite Dashboard
You can set favorite dashboards to make them accessible with a single select.
Procedure
- To set a favorite dashboard:
- To remove a favorite dashboard setting:
- To remove a favorite dashboard in one step:
- Access the Dashboard Browser.
- Select My Favorites, and select
, and then select
.
Set the Home Dashboard
The home dashboard is the first display that appears when Predix Essentials opens.
You can set the home dashboard from the dashboard browser or from the dashboard menu.
Dashboard Browser
The dashboard browser enables you to set the home dashboard from the list of dashboards displayed in My Favorites or All Dashboards.
Procedure
Results

What To Do Next

Dashboard Menu
The dashboard menu includes the option of setting a dashboard as the home dashboard. The menu is available when a dashboard is open in a tab.
Procedure
Results
Copy a Dashboard
Copy a dashboard to create a duplicate that can be customized to provide new asset monitoring capabilities.
About This Task
A copy of a dashboard includes the cards, widgets, tags, tag expressions, availability, metadata — everything except permissions — of the original dashboard. Default permissions are applied to dashboard copies.
Copies of instance-level, class-level, and contextless dashboards are the same type as the dashboard from which they were copied, with one exception: if an asset context has been selected for a contextless dashboard, the copy of the contextless dashboard becomes an instance-level dashboard.
You can copy any dashboard (other than General Dashboards), including those you do not have permission to modify. The copy will be modifiable.
Procedure
What To Do Next
Export a Dashboard
You can export a dashboard using a PDF to save the cards and widgets.
About This Task
You can export images of the cards and widgets in a dashboard view to a single-page PDF oriented in portrait format so you can create a report or for further analysis of the data.
Procedure
Enable or Disable Filter by Asset
About This Task
Procedure
- Access the Dashboard Browser.
- Select a dashboard from the Context Browser.
- Select
, and then select Edit Dashboard.
- To enable the filter, in the Card Library, move
to the right.
- To disable the filter, in the Card Library, move
to the left.
- Select Save to save the changes to your dashboard.
Enable or Disable Filter by Time Span
About This Task
Procedure
- Access the Dashboard Browser.
- Select a dashboard from the Context Browser.
- Select
, and then select Edit Dashboard.
- To enable the filter, in the Card Library, move
to the right.
- To disable the filter, in the Card Library, move
to the left.
- Select Save to save the changes to your dashboard.