Dashboard Cards
About Dashboard Cards
Cards add features to your dashboard.
Each default card contains functional widgets, some of which can be customized for your site needs.
- Two Generic Graph widgets.
- One Ambient Conditions widget.
- One Monitoring & Diagnostics widget.
- One Open Cases widget.
- One Unclaimed Alerts widget.
Custom cards require you to configure the layout and add widgets in the widget library.
- Add and update the configuration for widgets by modifying the card.
- Save the card to the card library.
- Access Time Control for the card.
- Rearrange the card order in the view.
- Delete a card.
- A single widget in a row.
- Two widgets in a row.
- Three widgets in a row.
Add and Delete Cards on a Dashboard
You can customize your dashboard by adding one or more cards in the card library.
About This Task
You can preview a card layout in the card library prior to adding it.
You can modify only one card at a time. You cannot select or navigate to another page when actively modifying a card. Actions for other cards on the view are disabled until you save or cancel the modifiers for the current card.
- When creating a new dashboard.
- To an existing dashboard.
- At the preview screen.
Procedure
Add and Hide a Dashboard Summary Card
You can add and hide a dashboard summary card with layout.
About This Task
Dashboard summary cards allow you to add widgets to layout tiles to help track statistics pertinent to the selected dashboard. Hiding a dashboard summary card does not delete the widgets or change the layout.
Procedure
- To hide a dashboard summary card:
- To add a dashboard summary card:
- Use the Context Browser to select an asset context.
- Select a dashboard that contains a dashboard summary card.
- Select
, and then select Edit Dashboard.
- In the Card Library, move
to the left.
- Select Save to save your changes.
What To Do Next
Create a Custom Card
You can design a card layout based on your needs and add it to a dashboard.
Before You Begin
About This Task
Custom cards allow you to add one to three columns per row, and an unlimited number of rows. However, you should limit the number of rows to three or four to maintain readability. Adding columns and rows changes the layout and affects the sizing of the widget tiles when added to the layout. You can add multiple custom cards to a view.
You can access cross-tenant asset resources that have been assigned to you. When selecting a an asset context, these resources are available for selection. If the resource you need is unavailable, contact your administrator.
Procedure
What To Do Next
Arrange Cards on a Dashboard
Arrange multiple cards on a dashboard into the order you want.
About This Task
You can change the order of cards on a dashboard.
Procedure
Save a Card to the Card Library
You can save a card to the card library as a template that is reusable, or a fixed context card.
Before You Begin
About This Task
Cards saved as a template can be blank, with no widgets assigned. You can then assign widgets when configuring the card. Cards saved as templates do not save context or data. However, cards saved as fixed context save both to the card.
Procedure
- Access the Dashboard Browser.
- Use the Context Browser to select an asset context.
- Select a view.
- In the card, select Action, and then select Save to Card Library.
- In the Upload section:
Modify and Delete Cards in the Card Library
You can modify and delete cards that have been saved to the card library.
Procedure
- To modify cards in the card library:
- To delete cards in the card library:
Export a Card
You can export a card as a PDF to save widget images and data.
About This Task
You can export images of the widgets and their data on a card in a dashboard view to a single-page PDF oriented in portrait format.
- Ambient Conditions
- Open Cases
- Unclaimed Alerts and Events
- Generic Graph Widget
- Interactive Graph Widget
- Monitoring & Diagnostics