Monitor Deployments
Monitor Predix (PAF) Runtime Deployments
You can monitor the status of the Predix runtime deployments in the Deployments page.
Procedure
- In the module navigation menu, go to Analytics > Deployments.The Deployments page appears.Based on the scheduling options, the status appears as follows in the LAST RUN column:
- For a deployment that are submitted with the Run Once scheduling option, the status appears as Success or Failed based on the actual run results.
- For a deployment that are submitted with the Recurrent scheduling option, the total successful asset jobs execution percentage appears as link in the the LAST RUN column, for example 100% Assets, and the success ratio of the last three runs appear in the SUCCESS RATIO column.
- To view the execution details of deployment with the Recurrent scheduling option, select the link in the LAST RUN column.A page that contains the details of the execution appears.Tip:
- To view the execution status of the assets for each run, as needed, select the Next Run or Previous Run button.
- To download the deployment result for each asset, in the Action column, select
.