Manage Analytic Data Flows
About Analytic Data Flows
Select and connect analytics from the analytics catalog to build analytic data flows.
Analytics Data Flows allow you to select analytics from the analytics catalog and place them into a specified order to run sequentially. All configuration information for the selected analytic is retrieved from the analytic template in the analytic catalog.
Each analytic added is considered a step in the analytic data flow. The inputs, constants, and outputs for the analytic are mapped on the I/O Mapping page. Each step in the data flow can contain multiple iterations of the step's I/O mapping.
When an analytic is created and added to the analytic catalog, a version is assigned to that analytic. For existing deployments which contain analytics whose version has been updated (single-step and/or within an Orchestration), and if the version has been marked as current, the deployment will then use the updated analytic version. The Analytics Data Flow section lists the version of the analytic being used for a particular analytic step in an orchestration.
Determine Analytic Versions
You can determine the analytic version being used within an Analytic Data Flow.
About This Task
Determining an analytic version for an analytic step in an Analytic Data Flow allows you to make decisions about modifying the orchestration based on that analytic version.
The analytic version refers to the analytic artifacts that were loaded into the analytic catalog. You can determine the version being used by analytic orchestration, and the user who loaded it into the analytic catalog. You can change the analytic version in an analytic orchestration data flow during deployment.
Procedure
- To determine the current analytic version in an analytic orchestration, do the following:
- To determine the analytic version of available analytic templates for use in orchestrations, do the following:
Add an Analytic to a Data Flow
You can add one or more analytics in the catalog to the data flow.
Before You Begin
About This Task
You can add multiple analytics to the data flow. When you add or drag an analytic to an existing data flow, the newly placed analytic links automatically to the adjacent analytics. Each added analytic is considered a step in a sequence. You cannot reorganize the items to modify the sequence of the data flow. However, you can delete analytics in the data flow and add them back in a different order.
Procedure
Modify an Analytic Data Flow
You can modify the analytic data flow to add existing analytic template.
About This Task
When you modify an analytics data flow, make sure that the orchestration is not deployed. Consider creating a new orchestration rather than modifying one that is in use.
- Modify the description.
- Add analytics in the Available Analytics list.
- Delete analytics in the Analytic Data Flow.
Make sure you add analytics in the order you want them to execute.
Procedure
- In the module navigation menu, navigate to .
- In the Search pane, select an existing orchestration to access its workspace.
- Hover over the existing description, then select on the Description box, then make your modifications, and then press ENTER or select outside the Description box.
- Select the Edit icon (
) in the Analytic Data Flow subsection of the Orchestration section.
- Add analytics or delete analytics in the data flow.
- Select Save to save your modifications.
Delete an Analytic in a Data Flow
You can delete an analytic step in an analytic data flow.
About This Task
Procedure
Modify the Analytic Version During Deployment
You can modify the analytic version being used within an Analytic Data Flow during deployment.
Before You Begin
You must have uploaded more than one analytic version to modify during the deployment of that analytic.
About This Task
Modifying the analytic version for an analytic step in an analytic data flow allows you to use a different version than set as current (default) in the analytic template.