Text Input
Use this plug-in to add a text box in your application.
The widget is available under designing application pages, drag-and-drop Text Input to a container.
. WhenText Box Properties
Field Name | Description |
---|---|
Target > Output Value | Provide the target data source to send information. |
Source > Input Value | Provide the input data source to receive values for the text box. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. The decimals will apply to Input Value, Minimum Value, and Maximum Value properties. |
Display Mode | Specify the input type for the taxt box, whether password, email or URL. |
Enable Clear Field Action | Select the check box to add a delete option in the end app to clear any data in the text box. |
Label Styling | Formats the text: Font Family, Font Size, and Font Color formats the text entered in the text box. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |